show the entry list
WinCC flexible ES -- Setting up development environments -- Installing and upgrading software
Which security measures help against unauthorized access to computer systems with WinCC flexible?
Compatibility Tool for Automation and Drive Technology
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
Why can you not select the installed languages in the Runtime Loader of PC Runtime?
When you install or uninstall WinCC flexible, why are some fonts no longer available for STEP 7 Basic V10.5?
How do you do an operating system update (OS update) on operator panels?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
What are the solutions offered for working with different versions of WinCC flexible?
What can cause the installation to abort or prevent successful starting of WinCC flexible?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
What might be the cause for not all the user interface languages being available for selection?
What might be the causes of unsuccessful MSDE installation (Microsoft Desktop Engine)?
What are the possible causes of the Setup program not starting for the installation of WinCC flexible?
How can you clear the cause of the message "Please reboot before installing any more programs"?
How do you uninstall WinCC flexible 2004?
How do you install ProAgent in SIMATIC WinCC flexible?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?
How can you install WinCC flexible from the hard disk?
WinCC -- Setting up development environments -- Installing and upgrading software
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
Why do I receive errors during the upgrade installation to WinCC version V7.0 SP2?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you switch the Microsoft SQL Server Management Studio Express to English on the bundle PC IPC 477C with WinCC V7.0 SP1?
Why does the installation of Microsoft SQL Server 2005 abort?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
How do you install WinCC V7.0 on a MUI operating system if the language set in Windows is not English?
What can you do if installation of Security Patch KB929046 fails in the Windows Server 2003 R2 SP2?
Why is it not possible to activate the subcomponent "Common" while installing the "Microsoft Message Queuing" component?
How can you install WinCC while the computer is logged on to a domain?
Why does installation of the "Microsoft Message Queuing Services" abort with an error message?
What is the difference between an upgrade and an update?
How do you upgrade the WinCC Options V6.1?
How do you upgrade WinCC V6.0 to WinCC V6.0 SP3?
How do you migrate WinCC V4.x projects to WinCC V6.x and WinCC V7.x?
How can you regularly receive updates to the latest versions of WinCC?
Which settings do you have to make to set up a redundant single-user station in Microsoft Windows XP SP2?
How can you analyze errors when installing WinCC?
Why is the Setup of SIMATIC WinCC aborted at the ACE component (Active Communication Environment)?
How should you proceed if installation of the Microsoft SQL server fails?
Missing SQLUNIRL.dll when Installing SIMATIC WinCC V6
Why does the SQL server 2000 SP3 not appear as present during the installation of WinCC V6.0 SP3, even though it is installed?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
Part number:

Fault description:
WinCC flexible 2008 is already installed and the WinCC V6.2 and WinCC V6.2 SP2 SQL server cannot be installed.

Cause:
A possible cause is the influence of the different SQL instances that are installed product-specifically with the installation of WinCC flexible or WinCC.

It is imperative that you keep to the following installation sequence when you install WinCC V6.2 or WinCC V6.2 SP2 and WinCC flexible 2008:

  1. WinCC V6.2 or WinCC V6.2 SP2
  2. WinCC flexible 2008

If you have already installed WinCC flexible 2008, consider the following procedure.

Remedy:
You can only install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 if the WinCC flexible instance of the Microsoft SQL Server 2005 Express Edition was deinstalled. WinCC flexible 2008 does not have to be deinstalled.

Procedure:
The table below describes the deinstallation of the WinCC flexible instance of the Microsoft SQL Server 2005 Express Edition:
 
No. Procedure
1 Deinstalling SQL instance
A complete deinstallation of WinCC flexible 2008 is not required.
  • Open the "Control Panel" of your operating system.
  • In the "Control Panel" click on "Software".
  • Select "Microsoft SQL Server 2005" and click on "Remove".


Fig. 01 - Remove program

2 Selecting Desktop Engine
  • Select "WINCCFLEXEXPRESS" in the opened dialog.
  • Click on "Next".


Fig. 02 - Select SQL-Instance

3 Finishing deinstallation
  • Click "Finish".
  • Reboot the PC after finishing the deinstallation.


Fig. 03 - Deinstallation of teh SQL-Instance

4 Installing WinCC and the SQL instance
  • Install WinCC V6.2 or WinCC V6.2 SP2
  • Start the "Setup.exe" file on the product DVD of WinCC flexible 2008 and execute the installation.
  • Accept the license agreements.
  • Click on "Next" and do not change the presettings in the following dialogs of the installation - see also Fig.04.

    Note:
    If the presettings are not changed only the WinCC flexible Instance of the Microsoft SQL Server 2005 Express Edition is installed.
     
  • Reboot the PC after installing the SQL instance for WinCC flexible 2008 again.


Fig. 04 - Installing SQL-Instance

Keywords:
Microsoft SQL Server 2005 SP1, Microsoft SQL Server 2005 SP2, Microsoft SQL Server 2005 Express

 Entry ID:30576253   Date:2008-09-11 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour