show the entry list
TeleService/TS/PC Adapter -- Setting up and parameterizing hardware -- Configuring devices
Which settings and parameters are required to create a gateway from GSM to ISDN with TeleService S7?
How do you parameterize the TS Adapter II / IE modems for Australia and New Zealand?
TeleService with ET200S (IM151-CPU) and TS Adapter
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
How is the TS Adapter IE parameterized for an EDI connection with the product PCAnywhere?
What should you watch out for when parameterizing the initialization string for a modem with TeleService?
How do you commission a GSM wireless modem of the type M20 Terminal with TeleService S7 V5.x?
How are remote monitoring and control performed with TeleService IE?
What are the options for using the TS Adapter IE as standard router?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you set the local modem after installing TeleService V6.1?
Check list for implementing a PC adapter
How do you commission the TS adapter V5.x with the GSM modules TC35 terminal and TC35i terminal?
Call-back feature of the TS adapter v.5.x
Connecting to the Network via Auxiliary System
SINAUT - Cellular Radio Components (GSM) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which firewall rules should you configure for the EGPRS router MD741-1 in order to have access to the Internet with the PG/PC from the LAN of the MD741-1?
Which firewall rules should you configure for the GPRS router MD740-1 in order to have access to the Internet with the PG/PC from the LAN of the MD740-1?
How can a GPRS connection be established to a SINAUT MICRO SC server if this has no static IP address?
How can you prevent the PROVIDER from automatically disconnecting the GPRS connection between a MD720-3 modem and SINAUT MICRO SS?
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
How do you reset the MD740-1 to the factory settings?
How do you parameterize the GSM modem MD720-3 for use with SINAUT ST7?
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
Part number:

Instructions
To set up communication between the TS Adapter II and the SINAUT GSM modem MD720-3, the following requirements must be fulfilled:

  • Firmware version of the TS Adapter II: V1.1.3 or higher
  • Version of the TeleService software: V6.0 SP1 or higher
  • Firmware version of the GSM modem MD720-3: V1.1.3 or higher
  • Hardware version of the GSM modem MD720-3: V3.3 or higher
  • No zero modem cable may be connected. The pin assignments must be 1:1 for a connection to the RS232 interface.

Note
The MD720-3 is not released in conjunction with the TS-Adapter V3.x and V5.x.

The table below describes the procedure for parameterizing the TS Adapter II for the SINAUT GSM modem MD720-3:
 
No. Procedure
1 The TS Adapter must be parameterized for the MD720-3 in order to set up a modem connection. The TS Adapter must be connected to the PC via a USB cable and the local connection must be set to direct connection (via USB).
  1. Open the PG/PC interface in the SIMATIC manager via "Options > Set PG/PC interface..." and set the access point "S7ONLINE (STEP 7)" for a connection to a TS Adapter I/II to the interface: "TS Adapter".
  2. Then click on the "Properties" button and choose the option field "Direct connection on:" in the "Local connection" tab.
  3. Choose "USB" from the drop-down list box.
  4. Save your settings in the PG/PC interface with OK.
2 In the SIMATIC Manager, start the teleservice options package via "Options > Teleservice" and open the parameterization interface of the TS Adapter with "Options > Parameterize Adapter I/II...". The "Assign TS Adapter I/II Parameters" dialog opens.
3 In the "Serial parameters" tab, set the transmission rate to 19200 bit/s.

Note
The GSM modem MD720-3 only works with the transmission rate of 19200 bit/s.

4 In the "Info" tab, check the version status of the GSM modem. If the SINAUT GSM modem and the RS232 interface of the TS Adapter are connected to the RS232 cable, the version status of the GSM modem can be read as in Fig. 01.


Fig. 01

You have to upgrade the firmware version if the GSM modem MD720-3 does not have at least the firmware version 1.7.3. More information on firmware updates for the SINAUT MD720-3 modem is available in Entry ID: 23067682.

Note
If you just get a "TIMEOUT" on the above-mentioned info page, then check the cable and the transmission rate. Set the transmission rate to 19200 bit/s, save the parameterization and then wait approximately 10 seconds. Afterwards, you have to call the "Assign TS Adapter I/II Parameters" dialog again.

5 Parameterize the TS Adapter in the "Network" tab with an address that has not yet been assigned in the network. The factory setting for the network address is 0 in the TS Adapter II. We recommend that you do not use the address 0, because PGs normally use the address 0 by default and so a conflict might arise when PGs are used.
  • The MPI address entered in the TS Adapter II must be the same as the programmed MPI address (parameter "MPI_TS_ADAPTER" of the FB48) in the STEP 7 user program.
  • The function block FB48 ("SMS_SEND") can only be used via the MPI interface of an S7 CPU.
  • The application is not possible via the PROFIBUS interface of an S7 CPU.
6 Change to the "Modem" tab. The initialization under "Modem Setting" should include the string "AT&FE1L1M1Q0V1&C1S0=1".  Fig. 02 shows the initialization string without PIN transfer for the SIM card used in the GSM modem. The setting shown is the factory setting.


Fig. 02

7 In the "Access Protection" tab, you have the option to set up an access protection for a teleconnection. Activate the access protection by defining the password for a user and/or a call back number.
8 Save and the close the "Assign TS Adapter I/II Parameters" dialog with OK. The parameterization of the TS Adapter II for the SINAUT GSM modem MD720-3 is then complete. For further information on connecting and starting the GSM modem, see
  • System manual GPRS/GSM modem SINAUT MD720-3
    (Entry ID: 23117745).

Creation environment
The pictures in this FAQ were created with TeleService Version 6.1.

Keywords
Terminal mode

 Entry ID:30330207   Date:2010-05-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour