show the entry list
Mobile Panels -- Product information -- Technical data and ordering information
Wich protective films can I use with SIMATIC HMI panels?
Where are the current declarations of conformity to be found for SIMATIC HMI panels (CE, UL, cUL, GOST)?
What should you watch out for when connecting the equipotential bonding to the connection box of a mobile panel?
How can you determine the "E-Stand" (hardware release) of an operator panel?
What is the power consumption or power dissipation of the SIMATIC HMI operator panels?
Which PROFINET services are supported by SIMATIC panels.
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
Which panels are certified for shipbuilding?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Which installation guidelines do you have to watch out for with the transponders for the Mobile Panel 227 IWLAN and the Mobile Panel 277F IWLAN?
Mobile Panel 170 can only be used with the connection box
Which Siemens department holds the EC conformity declarations for SIMATIC HMI?
Which SIMATIC Panels have the CCC certificate?
Which SIMATIC panels have or need an FCC certificate?
No yellow-red emergency stop switch on the Mobile Panel 170
No standard project in WinCE devices
Which installation guidelines do you have to watch out for with the transponders for the Mobile Panel 227 IWLAN and the Mobile Panel 277F IWLAN?
Part number:

Description:
The transponders and the Mobile Panel 277 IWLAN as well as the Mobile Panel 277F IWLAN communicate by radio waves exclusively in the 2.45 GHz area. This is irrespective of the WLAN Standard used (such as IEEE 802.11h / 5 GHz) between the Mobile Panel IWLAN and the access point. To ensure communication without interference, there should be no materials present that shield or absorb high frequency waves or they should only be present under certain conditions. For configuration and installation, you must consider the points described in detail in the PDF document - see attachment 1 - so that the field data in the operating instructions of the Mobile Panel 277 IWLAN and Mobile Panel 277F IWLAN is valid.


Fig. 01 - Mobile Panels and Transponder

Attachment 1: Mobile_Panel_Einbaurichtlinien_Transponder_e.pdf ( 307 KB )

Keywords:
Installation guidelines, Installation rules, Assembly, Arrangement

 Entry ID:30117468   Date:2008-08-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour