show the entry list
Industrial Ethernet PC software -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
What should I watch out for when using an "S/R OPC Server" in the Fetch/Write service mode?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do I create a Fetch/Write-connection (S5-compatible communication) to SIMATIC S7 for the SIMATIC NET-OPC Server via Ethernet with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Industrial Ethernet PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the ISO transport protocol?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Part number:

Instructions:
In this example, a CP1613 is used for the S5-compatible communication with an S5 controller on the Industrial Ethernet network.

Note:
The procedure described here also applies for communication processors CP1613 A2, CP1623, CP1612 and CP1512, as well as for commercially available network cards.

General information:
You do not need any other configuration software on the PC station. All the relevant applications are installed automatically along with the SIMATIC NET PC software.

If you are using a CP1613, then on the PC station, you need the license for the SIMATIC NET PC software S7-1613. This license key is also needed when using a CP1613 A2 or CP1623.

If you are using a CP1612, CP1512 or a commercially available network card, then on the PC station, you need the license for the SIMATIC NET PC software SOFTNET S7 Lean or SOFTNET S7.

Please follow the instructions below for configuring the PC station.

Guide_SRS5_Appl_e.pdf ( 607 KB )

Keywords:
Send, Receive, SOFTNET S7 Lean, SOFTNET S7 IE, S7-1613, CP1613, Network card, Guidelines, Configuration, CP1430

 Entry ID:29975605   Date:2008-07-24 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour