show the entry list
S7-300 CPU 31x -- Configuring and programming communication -- Using communication blocks
In STEP 7 V5.5, how do you read out the IP address of the S7-300 CPU in the user program?
What is the volume of data that you can transfer with function blocks FB34 "GET_E" and FB35 "PUT_E"?
How do you cyclically read out the 8 channels of the FM 350-2 counter module as quickly as possible?
How do you read out the IP address of the S7-300 CPU in the user program at runtime?
How do you enable the ad-hoc mode when you call the TRCV instruction?
How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the S7-300 and S7-400 CPUs and IM151-8 PN/DP CPU in STEP 7 Professional (TIA Portal)?
Which security modules can be reached with SOFTNET Security Client V4 over a secure IPsec tunnel connection?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Modbus blocks are already being used in the user program?
How do you implement chronological messaging with S7-300 CPUs and WinCC?
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
How can you read out diagnostics data from a SIRIUS 3RK3 modular safety system using a S7-300/400 CPU?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-300 CPUs and C7 complete devices?
How can you access via PROFIBUS DP another CPU, which is connected to the PROFIBUS DP as a slave, from a DP master using basic communication with SFC72 "I_GET" and SFC73 "I_PUT"?
How can you access consistent data without SFC14/15 as part of the process image?
ET 200S (standard modules) -- Configuring and programming communication -- Using communication blocks
When using the FB81 S_MODB on an S7-400 with more than 8 Kbytes of marker, how do you access the marker area above MB 255?
How do you set the input parameter TIME_RTS_OFF of the S_V24 instruction in the case of low data transfer rates?
How do you use the ET200S 1SI module in conjunction with a CPU S7-15xx?
How in WinAC MP 2008 do you program data transfer with the ET200S 1SI module for the 4-byte or 8-byte communication type?
Which CPU can you operate as a PROFINET I device?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
"Report System Errors" function can be used with ET 200S CPU from firmware version V2.1
Using the SFB75 (send alarm to the DP master) on an ET 200S CPU
ET 200pro -- Configuring and programming communication -- Using communication blocks
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
S7-400 CPU 41x -- Configuring and programming communication -- Using communication blocks
When using the FB81 S_MODB on an S7-400 with more than 8 Kbytes of marker, how do you access the marker area above MB 255?
How do you enable the ad-hoc mode when you call the TRCV instruction?
How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the S7-300 and S7-400 CPUs and IM151-8 PN/DP CPU in STEP 7 Professional (TIA Portal)?
How do you establish a redundant MODBUS/TCP communication over the integrated PROFINET interface of a CPU 41x-H in STEP 7 V5.5?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Modbus blocks are already being used in the user program?
How can you read out diagnostics data from a SIRIUS 3RK3 modular safety system using a S7-300/400 CPU?
Which communication options are there in SIMATIC S7?
How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication?
Consistent data in S7-400, summary of mechanisms
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you implement chronological messaging with S7-400 CPUs and WinCC?
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
How can you access consistent data without SFC14/15 as part of the process image?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-400 CPUs?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
Part number:

Description
You can use the open communication of the PROFINET for data exchange via the integrated Industrial Ethernet interface of a CPU, for example. The protocols below are supported for this:

  • TCP
  • ISO-on-TCP
  • UDP

The following communication blocks are available for "Open User Communication" via Industrial Ethernet using UDP Protocol:

  • FB65 "TCON" for connecting the UDP end point
  • FB66 "TDISCON" for disconnecting the UDP end point
  • FB67 "TUSEND" for sending data
  • FB68 "TURCV" for receiving data

These communication blocks are available in the Standard Library -> Communication Blocks.
Copy the latest versions of the above-mentioned communication blocks from the standard library into your user program and then call them in your user program.
The parameters for connecting the UDP end point are saved in a data structure. The data structure "OUCW_2" will be used in this example. This is stored in the DB1 data block and is parameterized by the user.

Note

  • Use the "Open Communication Wizard" for easy establishment of the UDP end point. This is available for downloading in Entry ID 98957840.
  • The TCP connection is not configured in NetPro.

Table 01 shows the "OUCW_2" data structure in which the parameters for establishing the UDP end point are stored.
 
Byte Parameter Data type Description
0 to 1 block_length WORD Length of the "OUCW_2" data structure
2 to 3 id BYTE Reference to this connection between user program and communication layer of the operating system
Value range: w#16#0001 to w#16#0FFF
You must specify the value of this parameter for the ID in the block concerned.
4 connection_type BYTE UDP protocol version: B#16#13
5 active_est BOOLEAN ID for how the connection is established
You must give the value FALSE to this parameter.
6 local_device_id BYTE Communication through the integrated PN interface of the CPU 315-2 PN/DP: B#16#02
7 local_tsap_id_len BYTE Length used for the local_tsap_id parameter: 2 bytes
8 rem_subnet_id_len BYTE This parameter is not used currently. It has the value B#16#00.
9 rem_staddr_len BYTE This parameter is not used currently. It has the value B#16#00.
10 rem_tsap_id_len BYTE This parameter is not used currently. It has the value B#16#00.
11 next_staddr_len BYTE This parameter is not used currently. It has the value B#16#00.
12 to 27 local_tsap_id ARRAY
[1 ..16] of BYTE
Local port number: 2000, for example
local_tsap_id[1] = B#16#7 (high byte of the port number in hexadecimal format)
local_tsap_id[2] = B#16#D0 (low byte of the port number in hexadecimal format)
local_tsap_id[3-16] = B#16#00
28 to 33 rem_subnet_id ARRAY
[1 ..6] of BYTE
This parameter is not used currently.
rem_subnet_id[1-6] = B#16#00
34 to 39 rem_staddr ARRAY
[1 ..6] of BYTE
This parameter is not used currently.
rem_staddr[1-6] = B#16#00
40 to 55 rem_tsap_id ARRAY
[1 ..16] of BYTE
This parameter is not used currently.
rem_tsap_id[1-16] = B#16#00
56 to 61 next_staddr ARRAY
[1 ..6] of BYTE
This parameter is not used currently.
next_staddr[1-6] = B#16#0
62 to 63 spare WORD Reserve, the parameter has the value W#16#0000.
Table 01

Description of the sample program
The S7 program contains the call of the FB65 "TCON" and the data structure "OUCW_2", in which the parameters for establishing the UDP end point are stored. The S7 program also includes the call of the function blocks FB67 "TUSEND" and FB68 "TURCV" from the Standard Library -> Communication Blocks. The FB67 "TUSEND" is for sending data to an S7 station, to a PC station, or to a third-party system. The FB68 "TURCV" is for receiving data from an S7 station, from a PC station or from a third-party system.

First create the hardware configuration for your S7-300 station. Configure Marker byte 100 as clock marker. The send job is triggered by this clock marker. Save and compile the hardware configuration of your S7-300 station and load it into the CPU.

The STEP 7 program consists of the blocks OB100, OB1, FB1, DB11, DB1, DB100, DB200 and FB63, FB64, FB67 and FB68.

OB100
The OB100 is a restart OB and is run when the CPU is restarted (warm start). In this OB the first communication trigger is enabled with marker M0.3.

OB1
OB1 is called cyclically. The FB1 is called in OB1 with the instance data block DB11, with the marker M0.3 as INIT_COM parameter and with the marker M10.0 as ABORT parameter. The marker M0.3 is reset in OB1 after the FB1 has been called.


Fig. 01

FB1
The FB1 is called cyclically in OB1. The following function blocks are called in FB1.

  • FB65 "TCON"
  • FB67 "TUSEND"
  • FB68 "TURCV"
  • FB66 "TDISCON"

Define connection number
You can change the connection number separately. Change the connection number in network 2 of FB1 in accordance with your configuration.
The connection number is stored in a static tag and so in the instance data block DB11.
The connection number "3" is defined in this example.


Fig. 02

Establishing the connection
Connection of the UDP endpoint is started by a positive edge at the input parameter "REQ" of FB65 "TCON". The "OUCW_2" data structure with the parameters of the local UDP end point is incorporated in the data block DB1.
On the input parameter "CONNECT" of the FB65 "TCON", the memory area is specified that contains the parameterization of the local UDP endpoint.
The connection of the UDP endpoint is set up at system start and remains until it is disabled with FB66 "TDISCON", the CPU goes into STOP mode, or the power supply is switched off.


Fig. 03

The send job is triggered by a positive edge on the input parameter "REQ" of the FB67 "TUSEND". The send request trigger is controlled by clock marker M100.6 and the variable "SEND_BUSY". If the send request is running, "SEND_BUSY" is set. It is then not possible to trigger a new send request.
You specify the memory area that contains the data to be sent at the input parameter "DATA".
You enter the number of bytes to be sent at the input parameter "LEN".
In this example the Send data is stored in DB100. 100 bytes of data is sent to the communication partner.
At the input parameter "ADDR" you specify the address of the data area where the recipient's IP address is stored. In this example, the address parameters of the communication partner are stored in the data structure "OUCW_3". This is incorporated in the data block DB1.
The output parameters "DONE", "ERROR" and "STATUS" are required for job evaluation.


Fig. 04

Table 01 shows the "OUCW_1" data structure in which the connection data is stored.
 
Byte Parameter Data type Description
0 to 3 rem_ip_addr ARRAY
[1 .. 4] of BYTE
IP address of the remote partner, such as 192.168.0.30
rem_ip_addr[1] = B#16#C0
rem_ip_addr[2] = B#16#A8
rem_ip_addr[3] = B#16#00
rem_ip_addr[4] = B#16#1E
4 to 5 rem_port_nr ARRAY
[1 .. 2] of BYTE
Remote number: 2000, for example
local_tsap_id[1] = B#16#7 (high byte of the port number in hexadecimal format)
local_tsap_id[2] = B#16#D0 (low byte of the port number in hexadecimal format)
6 to 7 spare ARRAY
[1 .. 2] of BYTE
Reserve, the parameter has the value W#16#0000.
Table 02

If the send request is successfully completed, "SEND_BUSY" is reset. A new send job can now be triggered.
If the send request is completed with an error, then "SEND_BUSY" is likewise reset and the value of the output parameter "STATUS" of the FB67 is saved for an error analysis.


Fig. 05


Fig. 06

The data can be received as soon as the UDP endpoint is connected.
With the input parameter "DATA", you specify the address and length of the data area where the received data is saved.
In this example 100 bytes of data are received and stored in DB200.
At the input parameter "ADDR" you specify the address of the data area where the sender's IP address is stored. In this example, the address parameters of the communication partner are stored in the data structure "OUCW_3". This is incorporated in the data block DB1. Table 02 shows the "OUCW_3" data structure.


Fig. 07

The output parameter "NDR" is for showing that new data has been received. The "RECV_LEN" output parameter indicates the length of the data received.
If the data is received successfully, then the value of the "RCVD_LEN" output parameter is saved.


Fig. 08

If the data is not received successfully, then the value of the "STATUS" output parameter is saved and evaluated.


Fig. 09

You can disconnect the UDP end point specifically with the FB66 "TDISCON". You start the job to disconnect the UDP endpoint with a positive edge at the input parameter "REQ" of FB66 "TDISCON".


Fig. 10

The STEP 7 project as a download
The STEP 7 project contains a sample program for calling FB1 and the function blocks FB65 "TCON", FB66 "TDISCON", FB67 "TUSEND" and FB68 "TURCV" with status evaluation. It was created with STEP 7 V5.5 SP3.

Sample_open_UDP.zip ( 290 KB )

Configuring additional TCP connections
To configure additional UDP endpoints, you copy the FB1 so that you receive another function block (such as FB101). Change the parameters and generate a new instance data block. Using the Open Communication Wizard you create a new data structure in which parameters of the new UDP end point are stored.

Further Information

  • Detailed information on open communication over Industrial Ethernet is available in the manual "System and Standard Functions for S7-300/400 Volume 1 and Volume 2" in Entry ID: 44240604.
  • Instructions for configuring a UDP connection for communication by way of S7-300 and S7-400 Industrial Ethernet CPs are available in Entry ID: 47885893.

 Entry ID:29738463   Date:2014-11-20