show the entry list
WinCC flexible ES -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Message indicator continues to be displayed despite counter at zero
How do you start a sound file via a script in the WinCC flexible PC Runtime?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages?
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
How do you display messages in WinCC flexible?
How can you evaluate the ACK button on a touch operator panel in WinCC flexible?
How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible?
How do you change and display SIMATIC WinCC flexible system events during configuration?
How can you change the ProTool default alarm window setting in WinCC flexible?
How can I acknowledge alarms in WinCC flexible via the PLC?
Why aren't messages output on the event recorder?
Why isn't the "Message display" shown in the foreground, but is covered by picture objects?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
How can you get the diagnostics buffer to be displayed in WinCC flexible?
Which settings need to be made in order to display alarm events after a specified point in time?
How can you create messages with externally preset texts as mass data and process them with Excel in WinCC flexible?
WinCC flexible RT -- Setting up systems -- Configuring software
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you simulate the system keyboard via K or F-keys?
How do you change the date format in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you configure the WinCC Autostart for WinCC flexible Runtime?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Touch Panel / Operator Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Two-line messages with S7-PDIAG and OP27/TP27
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Multi Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Mobile Panels -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Basic Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you integrate an HMI operator panel into a local network?
What transfer options are available in the various operator panels?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Pushbutton Panels -- Setting up and parameterizing hardware -- Setting up connections
What transfer options are available in the various operator panels?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Connecting PPs via PROFIBUS DP with the CP5431
Connection of a Pushbutton Panel to a S7-400H system via Y-Link
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
PP7 / PP17 with MPI on S7 200
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
Part number:

Description
This entry describes how to establish a direct connection between HMI Panels and frequency converters.

Please follow the instructions in the PDF file.

  direct_connection_HMI_frequency_converter_e.pdf ( 1584 KB )

Note
The SINAMICS G120 Control Units CU230P-2, CU240B-2 and CU240E-2 do not support the function described.

Additional Information
More related information is available in the Online Support at the links below.
 
Product Direct connection
HMI/Frequency converter
Frequency converter
Error lists for HMI
WinCC (TIA Portal) 58522638 47520881
WinCC flexible This entry

Note on security
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

 Entry ID:29522676   Date:2012-03-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour