show the entry list
WinCC flexible ES -- Product information -- General information
Does WinAC MP 2008 for WinCC flexible 2008 run in Windows 7?
Why can you not select the SIMATIC HMI Panel PC Ex as operator panel in WinCC flexible 2008?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which SQL servers are used by WinCC flexible? [Intranet] [Extranet]
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
Pushbutton Panels -- Setting up and parameterizing hardware -- Setting up connections
Which connector cables are available for connecting to SIMATIC Panels?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Connecting PPs via PROFIBUS DP with the CP5431
Connection of a Pushbutton Panel to a S7-400H system via Y-Link
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
PP7 / PP17 with MPI on S7 200
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Which GSDML files are there for the operator panels for Profinet IO?
Part number:

Configuration note:
If you have installed WinCC flexible and the STEP 7 Manager on your configuration computer, then the GSDML files of the operator panels that can be configured are already installed on the configuration computer.

Contents:

  1. Information on GSDML files
  2. Assigning and using the GSDML file
  3. GSDML files for Push Button Panels
  4. Link to the GSD files for Profibus DP

1. Information on GSDML files
All Profinet IO field devices are characterized by the Device Master File. In this file there are all the properties of the Profinet IO field devices that are relevant for the cyclical data exchange. The editing language of the device master data file used for Profinet IO is GSDML (General Station Description Markup Language), which is based on the XML model. The XML-based GSDML files are language-independent.

2. Assigning and using the GSDML file
The GSDML files for SIMATIC operator panels are required for the Profinet IO direct keys. This function is supported from WinCC flexible 2005 SP1.

After installing WinCC flexible and the STEP7 Manager, the following GSDML files for Profinet IO are included in the hardware catalog of the STEP7 Manager. No additional installation is necessary.
 
Operator panel as of WinCC flexible GSD file
Mobile Panel 177
OP177B
TP177B
2005 SP1 GSDML-V2.1-Siemens-HMI-20070612.xml
(older GSD file:)
GSDML-V2.1-Siemens-HMI-20070207.xml
Mobile Panel 277
MP277
OP277
TP277
2005 SP1
MP377 2007

Note:
The release version and the data of publication are also included in the name of the XML-based GSDML file. The release status depends on the version of WinCC flexible installed.

3. GSDML files for Push Button Panels
The downloadable GSDML file must be additionally installed in the HW config. of the STEP7 Manager.
You can find the GSDML files for Push-Button Panels in the link for the manuals under the small floppy disk symbol:
 
Operator panels Entry ID
Push Button Panel PP 17-I PN PROFIsafe
Push Button Panel PP 17-II PN
25023739

4. Link to the GSD files for Profibus DP
You can find information on the GSD files for Profibus under the following Entry ID 29339779.

Keywords:
Device master data files, general station description

 Entry ID:29339880   Date:2008-05-30 
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
User view