show the entry list
WinCC flexible ES -- Product information -- General information
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
Pushbutton Panels -- Setting up and parameterizing hardware -- Setting up connections
What transfer options are available in the various operator panels?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Connecting PPs via PROFIBUS DP with the CP5431
Connection of a Pushbutton Panel to a S7-400H system via Y-Link
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
PP7 / PP17 with MPI on S7 200
ProTool -- Product information -- General information
Which GSD files are there for the Profibus DP operator panels?
Which type of device has to be set in ProTool when using a SIMATIC panel PC x77?
How do you send customer projects to Technical Support?
Which Details does Technical Support need regarding Inquiries on ProTool/Lite/Pro and Operator Panels
Feedback on panels with ProTool V6.0
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Text display / Graphics devices -- Setting up and parameterizing hardware -- Setting up connections
What transfer options are available in the various operator panels?
Which GSD files are there for the Profibus DP operator panels?
Updating tags when a controller fails
What connecting cables are there for connections between the operator panels and the different controllers?
Testing the RS485 interface of a TD or OP
Which GSD files are there for the Profibus DP operator panels?
Part number:

Configuration note:
If you have installed ProTool or WinCC flexible on your configuration computer, then the GSD files of the operator panels that can be configured are already installed on the configuration computer.

Contents:

  1. Information on GSD files
    1.1 Language-dependent and independent GSD files
    1.2 GSD files for SIMATIC operator panels
  2. Storage paths of the GSD files
    2.1 GSD files for DP direct keys
    2.2 GSD files for S5 communication via Profibus DP
  3. Assigning and using GSD files
    3.1 GSD files for DP direct keys
    3.2 GSD files for S5 communication via Profibus DP
  4. GSD files for Push Button Panels
  5. Download of HMI GSD files
  6. Link to the GSDML files for Profinet IO

1. Information on GSD files
In the GSD files(General Station Description)  you get the communication characteristics of a PROFIBUS device. The GSD files get an ident number after certification from the Profibus user organization.

1.1 Language-dependent and independent GSD files
With GSD files for Profibus DP you distinguish between language-dependent and independent GSD files. The language-independent GSD files are defined by the extension "*.gsd". Language-dependent GSD files are characterized by the language-related extension of the GSD file.
 
No.

Extension

Language
1 *.gsg German
2 *.gse English
3 *.gsf French
4 *.gsi Italian
5 *.gss Spanish
Table 01 - extensions of language-dependent GSD files

1.2 GSD files for SIMATIC operator panels
For SIMATIC operator panels there are two different GSD files. These GSD files are not different in name but in application.

There are GSD files for:

  • DP direct keys for S7 controllers
  • S5 communication via Profibus DP

The contents of a GSD file can be verified with a data editing program such as "Notepad". The two GSD files of the same name differ through the user-defined modules. If modules such as "Class B tiny" and "Class B small" are included, then it is a GSD file for S5 communication via Profibus DP.

2. Storage paths of the GSD files
There are two different GSD files for the SIMATIC Panels. You will find further information under Point 1.2.

2.1 GSD files for DP direct keys
If in addition to ProTool or WinCC flexible the STEP 7 Manager was successfully installed on the configuration computer, then the GSD files for the DP direct keys are already included in the hardware catalog in the HW config of the STEP 7 Manager. No additional installation is necessary.

2.2 GSD files for S5 communication via Profibus DP
For the S5 communication via Profibus DP you have to add the required GSD files to your configuration software (for example COM Profibus).

The GSD files of the SIMATIC operator panels for the S5 communication via Profibus DP are installed on your PC under one of the following paths:

ProTool:
C:\Program Files\Siemens\PROTOOL\PLCProg\GSD
or
C:\Programs\Siemens\PROTOOL\PLCProg\GSD

WinCC flexible:
C:\Program Files\Siemens\SIMATIC WinCC flexible\WinCC flexible Support\PlcProg\GSD
or
C:\Programs\Siemens\SIMATIC WinCC flexible\WinCC flexible Support\PlcProg\GSD

3.Assignment and use of the GSD files
There are two different GSD files for the SIMATIC Panels. You will find further information under Point 1.2.

3.1 GSD files for DP direct keys
The GSD files for the DP direct keys have the same designation including extension as is listed in the table - see 3.2 - below.

3.2 GSD files for S5 communication via Profibus DP
After successful installation of ProTool or WinCC flexible these GSD files are available on your configuration computer for the S5 communication via Profibus for the following operator panels:
 
Operator panel GSD file Path under
OP5 si058020.gsd ProTool
OP7 DP
OP17 DP
si078020.gsd ProTool
OP7 DP 12
OP17 DP 12
si078040.gsd ProTool
TD10
TD20
OP20
si108020.gsd ProTool
OP15 si158020.gsd ProTool
TD17 si178040.gsd ProTool
OP25
OP35
si258020.gsd ProTool
OP27
OP37
TP27
TP37
si278040.gsd ProTool
TP170B
OP170B
Mobile Panel 170
Siem80B3.gsd ProTool & WinCC flexible
MP370 Siem80BE.gsd ProTool & WinCC flexible
MP270B
OP270
TP270
Siem80E4.gsd ProTool & WinCC flexible
PC Siem8076.gsd ProTool & WinCC flexible
OP 37/PRO Siem8077.gsd ProTool
MP270 Siem8078.gsd ProTool & WinCC flexible
OP77B
OP177B
TP177B
Mobile Panel 177
Siem8107.gsd WinCC flexible
OP277
TP277
MP277
Mobile Panel 277
Siem813F.gsd WinCC flexible
MP377 Siem815A.gsd WinCC flexible

Note:
On the computer there are only GSD files that can be configured with the installed Engineering Software.

4. GSD files for Push Button Panels
You can use the links to GSD files listed below both for communication to S5 and to the S7 controllers via Profibus DP.
You find the GSD files for Push-Button Panels in the link for the manuals under the small floppy disk symbol:
 
Operator panels Entry ID
Push Button Panel PP 7
Push Button Panel PP 17-I
Push Button Panel PP 17-II
1142916
Operator panel PP 17-I PROFIsafe 21913151

Note:
You will find information on GSD files Push Button Panels for Profinet under the following Entry ID: 29339880.

5. Download of HMI GSD files
You will find the GSD files for S5 communication as a download under the Entry ID 39329178.

6. Link to the GSDML files for Profinet IO
You will find information on the GSDML files for Profinet IO under the following Entry ID 29339880.

Keywords:
Device master data file, general station description

 Entry ID:29339779   Date:2008-05-30 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour