show the entry list
WinCC -- Configuring alarms and messages -- Configuring Alarm Logging
How do you calculate the memory requirement of a server or central archive server (CAS)?
How can I create a message in WinCC if, when backing up an archive, the backup path is not available, cannot be reached or the data medium is full?
How can you switch off the message 1000915 "Terminal adapter <MAC-address> disconnect"?
How can I avoid the whole screen being filled when I open a picture using the OpenPicture function via LoopInAlarm?
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Which functions do the different variable types have for the individual messages?
How can you get specific messages to flash in the alarm list until the user has acknowledged them?
What format is best suited for defining the AlarmLogging-event variables?
What do you do if alarms are not displayed at Runtime?
How can you assign the functions of the toolbar buttons of WinCC Alarm Logging OCX to external buttons?
How can I delete individual messages from a group message?
When are alarms initiated by the limit monitoring in WinCC if the limit values are supplied indirectly?
What should I watch out for when assigning the names of message types, message classes and group messages?
Why isn’t there display of the "Comment" toolbar button of the Alarm Logging Control in Runtime?
How can you display process values formatted in an Alarm Logging message line?
How can I change the state texts of the message classes from +, -, * to actual text of my own?
How can you check the configuration of the Alarm Logging to see whether there is multiple use of message, status and acknowledge tags or whether the message tags are not configured?
At Runtime, how can you determine the message texts or process-associated values when a message appears in the associated, user-specific action "GMsgFunction()"?
How do you display and operate alarms in Runtime?
What is the structure of the format instruction for displaying the contents of WinCC tag values at Runtime in the user text blocks of a message?
How can you create messages whose message texts consist of a fixed part and a variable part?
What do the statuses of the status and acknowledge tags look like in the Alarm Logging?
What statuses can a message go through at Runtime?
How can I use the limit-value monitoring function of Alarm Logging to monitor the free drive space of a hard disk?
Why after WinCC Runtime starts is a message displayed with the text "..... already used"?
How can you configure user-defined message classes?
How can you change the acquisition cycle of the WinCC Alarm Logging?
How can you use the status tag of a message?
What should you watch out for in particular with the "Loop in Alarm" function?
How can you export, change and then reimport message texts?
What should I watch out for when assigning the names of message types, message classes and group messages?
Part number:

You must give unambiguous names to message types, message classes and group messages. For example, you must not use the same name for a message class and a group message.

 Entry ID:2908340   Date:2000-08-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour