show the entry list
Touch Panel / Operator Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Two-line messages with S7-PDIAG and OP27/TP27
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
ProTool Option - ProAgent -- Setting up development environments -- Configuring the software
Two-line messages with S7-PDIAG and OP27/TP27
S7 GRAPH sequencers or PDIAG watchdogs (also movements) do not work.
Process values in PDIAG or S7-GRAPH messages
S7 Graph sequencers are not offered as a diagnostics-supporting unit in ProTool.
Message classes/message blocks created/renamed in STEP 7 are overwritten in the ProAgent generation run
Deactivating the operating mode display in ProAgent on the OP
ProTool/Pro-ProAgent default images for all operator panels and panel PCs
Message: "W5509: illegal device identification 0" when generating a ProTool project with ProAgent diagnostics pictures
No display of message texts and unit names in the  ProAgent standard pictures of ProTool Runtime
Message: "W3799 Internal message: Can not find Motion Unit for Unit ..." when generating a ProTool project with ProAgent diagnostics images
Inserting the ProAgent standard program into the existing program.
Two-line messages with S7-PDIAG and OP27/TP27
Part number:

QUESTION:
How can you configure two-line messages in S7-PDIAG?

ANSWER:
When configuring message texts in S7-PDIAG, the formatting character "\n", known from ANSI C, is inserted at the point in the text where the line break is supposed to be. The line break is also displayed correctly in the "CPU messages" window.

 Entry ID:2907670   Date:2000-08-25