Consistent data, overview and application in distributed I/O. In the following is a description of how to deal with consistent data in STEP 7.
28991143_Consistent_Data_e.pdf ( 766 KB )
The entries dealing with the topic of consistent data are listed below.
|
Topic |
Entry ID |
|
Definition of terms. |
5116353 |
| How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device? |
21848242 |
| Consistent data in S7-400 |
11646774 |
| How can you access consistent data without SFC14/15 as part of the process image? |
8751062 |
| How is consistent data of the distributed I/O processed in S7 masters? |
245111 |
| Rules for the CPU 315-2 DP accessing the distributed I/O |
42413 |
| CP 342-5 -- How can you read and write consistent data of a DP slave via the CP 342-5? |
21627748 |
| What should you watch out for when configuring consistent data in COM PROFIBUS with IM 308-C as DP slave? |
22566679 |
| What are the options for address assignment of consistent data in IM 308-C? |
21459883 |
Keywords:
SFC 14, SFC 15, Consistency
|