show the entry list
STEP 7 -- Setting up and parameterizing hardware -- Setting up modules for distributed operation
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How can you conveniently change the IP parameters and PROFINET IO device names using a program in STEP 7 V5.5?
Configuring an ET200U always with an even number of modules
How do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET?
How is consistent data of the distributed I/O processed in S7 masters?
What are the differences between the GSD files and the integrated metaknowledge in the HW Config?
What should you watch out for during configuration with GSD files for DPV0 and DPV1 slaves?
Information about "Setting up modules for distributed mode"
How can you keep data blocks, markers, timers and counters remanent in an IM151 CPU in the case of a power failure?
Why is the generation of the "Report System Error..." function interrupted whenever a module is used with GSDML file V2.0?
What should you watch out for with regard to subrack failure when programming the OB86?
How do you enter comments for DP slaves in the HW Config?
How can you easily print the labeling strips of the S7 I/O?
PROFIBUS general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
Which options are available for configuring the ET 200 stations?
Configuration of the alarm mode in STEP 7 for the diagnostics repeater (6ES7 972-0AB01-0XA0)
Correction to bus time calculations
Basic knowledge for configuring PROFIBUS-DP networks
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Cyclic program processing only once all the DP stations have signaled that they are finished
Which parameters must be taken into account when planning an electrical network?
How can you calculate the bus cycle time on the PROFIBUS DP with STEP 7?
PROFINET general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
What should you watch out for when you configure the I device and the higher-level IO controller in the same STEP 7 project?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you reset the IP address and device name of an I device?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
What should you watch out for in the configuration when data is exchanged via Industrial Ethernet in parallel via I/O addresses and TCP and UDP connections?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
Assigning names and addresses in PROFINET IO
Which options are available for configuring the ET 200 stations?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Connecting an S7-300 to a DP/PA-Link
S7-400 CPU 41x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How can time and date be acquired from a GPS signal?
How do you configure time synchronization?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can I procure the GSD files for my S7-400 CPUs?
How do you do a cold start with SIMATIC S7-400 CPUs version V4.0 and higher?
Why should you switch the operating mode of the CPU from Test to Process after commissioning the STEP 7 program?
How do you use or update process image partitions for S7-400 CPU modules during an interrupt OB?
Only up to 27 configured blocks are displayed
What should you watch out for with the "forcing inputs" function in the S7-400?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
Part number:

Configuration Notes
From STEP 7 V5.4 SP2 onwards, STEP 7-external tools (Device Tools) are integrated for parameterizing and diagnosing distributed I/O devices via the Tool Calling Interface (TCI) in STEP 7. The following distributed devices are concerned:

  • PROFIBUS DP V1 Slave
  • PROFINET IO devices

Requirements

  • The device tool must support the TCI specification. TCI is a calling interface specified by PROFIBUS & PROFINET International (PI). You can use the TCI calling interface to transfer configuration from the Engineering Tool to the Device Tool.
  • The device tool and STEP 7 have to be installed on the same computer.

You have the following options for connecting the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices via the TCI calling interface.

SIMATIC Field PG is connected to the same bus system as the distributed I/O devices


Fig. 01: SIMATIC Field PG and distributed I/O devices in the same bus system

SIMATIC Field PG is not connected to the same bus system as the distributed I/O devices
It is possible to parameterize and diagnose the distributed I/O devices from a different bus system via the TCI calling interface.
Here you need a data record gateway. The modules below support the data record routing function and can thus be implemented as data record gateway.
 
Module Order number Firmware
IE/PB Link 6GK1411-5AB00
6GK1411-5AA00
-
CPU412-2 PN 6ES7412-2EK06-0AB0 from V6.0
CPU414-3 PN/DP 6ES7414-3EM05-0AB0 from V5.1
CPU414-3(F) PN/DP 6ES7414-3EM06-0AB0
6ES7414-3FM06-0AB0
from V6.0
CPU416-3(F) PN/DP 6ES7416-3ER05-0AB0
6ES7416-3FR05-0AB0
from V5.1
CPU416-3(F) PN/DP 6ES7416-3ES06-0AB0
6ES7416-3FS06-0AB0
from V6.0
CP443-5 Extended 6GK7443-5DX04-0XE0 from V3.0
CPU319-3(F) PN/DP 6ES7318-3EL00-0AB0
6ES7318-3FL00-0AB0
from V2.7
CPU319-3(F) PN/DP 6ES7318-3EL01-0AB0
6ES7318-3FL01-0AB0
from V3.2
CPU317-2(F) PN/DP 6ES7317-2EK14-0AB0
6ES7317-2FK14-0AB0
from V3.1
CPU315-2(F) PN/DP 6ES7315-2EH14-0AB0
6ES7315-2FJ14-0AB0
from V3.1
IM151-8(F) PN/DP CPU with DP master module 6ES7138-4HA00-0AB0 6ES7151-8AB00-0AB0
6ES7151-8FB00-0AB0
from V2.7
IM151-8(F) PN/DP CPU with DP master module 6ES7138-4HA00-0AB0 6ES7151-8AB01-0AB0
6ES7151-8FB01-0AB0
from V3.2
IM154-8(F) CPU 6ES7154-8AB01
6ES7154-8FB01
from V3.2

You can parameterize DP slaves connected to the PROFIBUS from the MPI network or from the Industrial Ethernet via the data record gateway.


Fig. 02: Parameterizing DP slaves from MPI / Industrial Ethernet

 Entry ID:28879514   Date:2011-04-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour