Requirements: The requirement for configuring Asian fonts in WinCC flexible is Microsoft Windows 2000 Professional or Windows XP Professional. You do not explicitly need an English version of either system with Multilingual User Interface (MUI). You only need an MUI-compatible operating system if you wish to change the interface language of Windows.
Note:
With regional versions of Microsoft Windows, you can only install Asian keyboards and Asian fonts. You cannot change the interface language of Microsoft Windows.
The Asian versions of Microsoft Windows already support Asian languages, so you do not need to make any more settings in the operating system.
Here, we explain the installation and settings for
which you need for creating a "Simplified Chinese" configuration with WinCC flexible.
The procedure for Traditional Chinese, Korean and Japanese is the same.
Note:
You need to make more settings in the operating system when using Asian fonts in ProTool. More information is available in Entry ID: 2182387.
Settings in Windows 2000 Professional Please note that you need administrator rights for making settings in Windows 2000.
| No. |
Procedure |
| 1 |
Retro-installation of "Simplified Chinese" in Windows 2000 (English)
- Open the "Regional Options" item in the Control Panel.
- Select the "General" tab and under "Language settings for the system" set a check mark for "Simplified Chinese".
  Fig. 01 - Regional Options - General
| => |
The data (from the Windows 2000 Professional CD) is retro-installed and then you must do a Restart. | |
| 2 |
Add input locale
- Switch to the "Input Locales" tab and under "Installed input locales" click on "Add...".
  Fig. 02 - Regional Options
|
| 3 |
Select input locale
- Under "Input locale:" you select the setting "Chinese (PRC)".
- In the "Keyboard layout/IME" field, you select the IME (Input Method Editor) "Chinese (Simplified) - QuangPin" and acknowledge the settings with "OK".
  Fig. 03 - Input locale and IME
- Click "OK" to close the "Regional Options" dialog.
| => |
The data (from the Windows 2000 Professional CD) is retro-installed and then you must do a Restart. | |
| 4 |
Change keyboard layout/IME in Windows 2000
- Click on the IME icon in the toolbar (taskbar) of Windows 2000.
- Select the Chinese keyboard layout (IME) in the pop-up menu.
  Fig. 04 - Select keyboard layout
Specific settings are necessary in the WinCC flexible project for entering Chinese fonts. More information about this is available in the section "Settings in WinCC flexible" below. |
Settings in Windows XP Professional Please note that you need administrator rights for making settings in Windows XP.
Settings in WinCC flexible In the following section we explain all the steps necessary for entering and displaying Chinese characters in WinCC flexible ES and RT (Runtime).
Note: If you need the interface language, i.e. menus and dialogs, for configuring in Chinese in WinCC flexible, then change or install the relevant interface language.
You need WinCC flexible 2004 ASIA and WinCC flexible 2005 ASIA respectively for WinCC flexible 2004 and 2005. Note that you cannot install all the editions of WinCC flexible and WinCC flexible ASIA on one operating system.
The Asian interface languages are available in all editions from WinCC flexible 2007 onwards. All the interface languages available can be retro-installed with the product CD of WinCC flexible.
More information changing the interface language is available in Entry ID 18922331.
| WinCC flexible |
Languages |
| Version |
German, English,
French, Italian, Spanish |
English,
Chinese (simplified), Chinese (traditional), Korean, Japanese |
| 2004 |
X |
|
| 2004 ASIA |
|
X |
| 2005 |
X |
|
| 2005 ASIA |
|
X |
| From 2007 onwards |
X |
X |
Table 01 - Languages available for the different versions of WinCC flexible
Keywords:
MUI = Multilingual User Interface, Language settings, Configure in multiple languages, System settings, Language import, Language export, Language extension
|