show the entry list
Network transitions and links (DP) -- Product information -- System description
What is the difference between "normal routing" and data record routing?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What are the requirements for operating the DP/ASi-Link Advanced as DP master on a CP 443-5 Extended?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What are the requirements for using the S7 routing function and which modules can you implement?
How is the DP/PA link structured?
Unidirectional data transfer with the DP/DP coupler
Documentation for the DP/PA coupler in Dutch, Danish, Finnish, Swedish, Portuguese and Greek
What are the requirements for operating the DP/ASi-Link Advanced as DP master on a CP 443-5 Extended?
Part number:

Configuration Notes:
The following requirements must be fulfilled to operate the DP/ASi-Link Advanced (6GK1415-2BA10 or 6GK1415-2BA20) on a CP 443-5 Extended (6GK7 443-5DX03-0XE0) or CP 443-5 Extended (6GK7 443-5DX04-0XE0).

  • Use the following firmware versions:
Communications processor Firmware
6GK7 443-5DX03-0XE0 from V5.2 onwards (see Entry ID: 27201492)
6GK7 443-5DX04-0XE0 from V6.3 onwards (see Entry ID: 26372646)
  • Configure the appropriate module from the hardware catalog in the STEP 7 hardware configuration.

 Entry ID:28813823   Date:2008-04-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour