Description: The file system is for storing HTML files, applets and other user-specific files. The relevant files can be transferred to the modules by FTP (File Transfer Protocol). The file system is supplied from the factory filled with default files. If you intend to delete the whole file system and start again in the output status, you can start formatting with the web browser (e.g. Internet Explorer) with the following command as described in the device manual:
http://<IP address>/__FSys_Format With this command you must observe uppercase and lowercase lettering.
The following prompt for input is displayed after the command has been executed.

Fig. 01: Input prompt after http://<IP address>/__FSys_Format
Access to the FTP file system is protected by relevant rights and a password to prevent unauthorized manipulation of the FTP file system. For this reason, you must configure a user with appropriate rights in the STEP 7 configuration, who is permitted to access the FTP file system.
The user needs at least the following authorization:
- Access with FTP to files in the S7 station.
Configuring a user: In the following we configure a user with administrator rights in the STEP 7 configuration. In the Hardware Configuration you open the Properties dialog of the Industrial Ethernet CP. Switch to the "Users" tab. Click the "Add..." button to create the new user.

Fig. 02: Properties dialog IE CP -> "Users" tab
In the following dialog you enter the user name for the user. As administrator, the users receives authorization for all possible functions. Click the "Password" button.

Fig. 03: Defining user rights
Define the password for the user just added.

Fig. 04: Defining a password
The user is activated automatically when the configuration is downloaded from STEP 7. Entering the relevant password provides unlimited access.
Installing a new FTP file system: After formatting, the file system is completely empty. This means that also factory-installed files are no longer available.
The file systems for the IE IT and Advanced CPs are available for downloading in the Entry IDs listed below. After downloading, you must transfer the files to the Industrial Ethernet CP by FTP.
| IE CP |
MLFB |
Entry ID |
| CP343-1 IT |
6GK7343-1GX11-0XE0 |
9970816 |
| CP343-1 Advanced |
6GK7343-1GX21-0XE0 |
19026376 |
| CP343-1 Advanced |
6GK7343-1GX30-0XE0 |
37724805 |
| CP443-1 IT |
6GK7443-1GX11-0XE0 |
9970816 |
| CP443-1 Advanced |
6GK7443-1EX40-0XE0 |
19280136 |
| CP443-1 Advanced |
6GK7443-1EX41-0XE0 |
36843304 |
| CP443-1 Advanced |
6GK7443-1GX20-0XE0 |
36842095 |
|