Configuration Notes:
SIMATIC PCS 7 V6.1 SP2 is not released for the following PCS 7 OS migration products:
- PCS 7/APACS+ OS V6.1
- PCS 7/90 OS V6.1
- PCS 7/505 OS V6.1
- PCS 7/PVX OS V6.1
Please install SIMATIC PCS 7 V6.1 in each case from the Toolset DVD that is supplied with the corresponding PCS 7 OS migration product (SIMATIC PCS 7 V6.1 + SP1).
Proceed as follows if you wish to use a SIMATIC PCS 7 Industrial Workstation (OS, ES/OS, Client) of the Rack PC 547B type preconfigured with SIMATIC PCS 7 V6.1 + SP2 for one of the above-mentioned migration products.
- First install the operating system from the Restore DVD A1 (Windows Image).
- Then install SIMATIC PCS 7 V6.1 + SP1 from the PCS 7 Toolset DVD supplied with the PCS 7 OS migration products.
|