show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
Part number:

Configuration Notes
The CP443-1 (6ES7443-1EX20-0XE0 V1.0) is the successor product to the CP443-1 (6GK7443-1EX11-0XE0).
The delivery release of CP443-1 (6GK7443-1EX20-0XE0 V1.0) is available in Entry ID: 26685738. According to the delivery release the CP443-1 (6GK7443-1EX20-0XE0 V1.0) can be configured as from STEP 7 V5.4 SP3 plus Hardware Support Package (HSP).

When replacing module CP443-1 (6GK7443-1EX11-0XE0) with CP443-1 (6GK7443-1EX20-0XE0) you must modify the hardware configuration of your S7-400 station in STEP 7 in order to be able to use the additional functions of CP443-1 (6GK7443-1EX20-0XE0).

If the CP443-1 (6GK7443-1EX11-0XE0) is configured in STEP 7 V5.4 SP3 and is replaced with a CP443-1 (6GK7443-1EX20-0XE0 V1.0), the parameters listed below are not adopted automatically:

  • The configured MAC address.
  • The configured IP address.
  • The configured subnet mask.
  • The information about which network the module is connected to.
  • The fixed settings of the Ethernet port.
  • Connection information of the S7 connections in NetPro.

Proceed as follows for replacing the CP443-1 (6GK7443-1EX11-0XE0) with the CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3.
 
No. Procedure
1 Open the hardware configuration of the S7-400 station where the configured CP443-1 (6GK7443-1EX11-0XE0) is to be replaced with the CP443-1 (6GK7443-1EX20-0XE0).

Double-click on the CP443-1 (6GK7443-1EX11-0XE0) located in the rack. The Properties dialog of the CP opens.


Fig. 01

2 In the Properties dialog of the CP you click on the "Properties" button. The "Properties - Ethernet Interface CP443-1" dialog box opens.


Fig. 02

3 In this example the following IP address parameters are defined for the CP443-1 (6GK7443-1EX11-0XE0):
  • MAC address: 08-00-06-01-36-01
  • IP address: 140.90.36.1
  • Subnet mask: 255.255.0.0
  • The module is connected to subnet "Ethernet(3)".

In the "Properties - Ethernet Interface CP443-1" dialog you define the IP address parameters for the CP443-1 (6GK7443-1EX11-0XE0).


Fig. 03

4 Note the IP address parameters that are defined for the CP443-1 (6GK7443-1EX11-0XE0).
5 Replace the configured CP443-1 (6GK7443-1EX11-0XE0) with the CP443-1 (6GK7443-1EX20-0XE0), i.e. select the CP443-1 with order number 6GK7443-1EX20-0XE0 in the Hardware Catalog under "SIMATIC 400 > CP-400 > Industrial Ethernet > CP443-1" and drag-and-drop this to the configured CP443-1 (6GK7443-1EX11-0XE0) in the rack.


Fig. 04

6 When you replace the CP443-1 (6GK7443-1EX11-0XE0) with the CP443-1 (6GK7443-1EX20-0XE0), the "Properties - Ethernet interface PN-IO" dialog opens.


Fig. 05

Note
The IP address parameters set for the CP443-1 (6GK7443-1EX11-0XE0) are not adopted automatically for the CP443-1 (6GK7443-1EX20-0XE0), i.e.:

  • The MAC address configured for the CP443-1 (6GK7443-1EX11-0XE0) is deactivated.
  • A default IP address with associated subnet mask is assigned for the CP443-1 (6GK7443-1EX20-0XE0). These IP address parameters are different to those configured for the CP443-1 (6GK7443-1EX11-0XE0).
  • The CP443-1 (6GK7443-1EX20-0XE0) is not assigned to any subnet.
7 Manually set the IP address parameters noted in Step 4 and close the "Properties - Ethernet interface PN-IO" dialog with "OK".


Fig. 06

8 Now the message below is displayed.


Fig. 07

Acknowledge this message with "No". This completes module replacement in the hardware configuration.

The additional functions of CP443-1 (6GK7443-1EX20-0XE0) mean that there are more dialogs in the Hardware Configuration for the configuration of the CP443-1 (6GK7443-1EX20-0XE0) than for the configuration of the CP443-1 (6GK7443-1EX11-0XE0). There are three other dialogs in addition to the Properties dialog with CP443-1 (6GK7443-1EX20-0XE0):

  1. PNIO - Properties of the PN-IO interface
  2. Port1 - Properties of the first LAN port
  3. Port2 - Properties of the second LAN port

With the CP443-1 (6GK7443-1EX20-0XE0) the dialog for setting the address parameters is no longer available in the Properties dialog of the module, but in the Properties dialog of the PN-IO interface. You can see this clearly in the following figure.


Fig. 08

 Entry ID:28370152   Date:2010-08-16 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour