Mostrar lista de artículos
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
Which can be connected directly to a panel?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Floppy disk drive on OP 15, OP 17 and C7-624
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Cable for loading the configuration onto OP/TP
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Text display / Graphics devices -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
Floppy disk drive on OP 15, OP 17 and C7-624
Floppy disk drive on OP 15, OP 17 and C7-624
Referencia:

QUESTION:
I want to connect a floppy disk drive to an OP 15, OP 17 or to a C7-624 for recipe management. Is that possible?

ANSWER:
There is an FD20 floppy disk station for these devices.
This station is sold by the Sympat company in Nuremberg.

Sympat GmbH
Fürther Str. 212
D-90429 Nürnberg
Tel. +49-911-32294-0
Fax. +49-911-3189146

E-Mail: info@sympat.de
URL: www.sympat.de

 Nr. de identificación (ID):283393   Fecha:1998-03-30