show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
What should you watch out for with the PPI/MPI/DP interfaces if you want to use the CP 5711 with a SIMATIC S7-200?
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Part number:

Description
Below is a description of the settings you must make for configuring a connection between panels or WinCC flexible PC Runtime and S7-200.

Please follow the instructions in the PDF file (Attachment 1). The following points are covered in the document.

1 Connection via PROFIBUS
    1.1 Configuration in WinCC flexible
    1.1.1 Settings in the configuration
    1.2 Settings in STEP 7 Micro/WIN
2 Connection via Ethernet (CP243-1)
    2.1 Requirements
    2.1.1 Connection between S7-200 and WinCC flexible PC Runtime
    2.1.2 Connection between S7-200 and Windows-based operator panels
    2.2 Configuration of CP 243-1 with STEP 7 Micro/WIN
    2.3 Configuration
    2.3.1 WinCC flexible PC Runtime
    2.3.2 Windows-based operator panels
3 Connection via RS232/ PPI cable
    3.1 Connection between WinCC flexible PC Runtime and an S7-200 controller
4 Connection via TeleService
    4.1 Requirements
    4.2 Direct connection between a TS Adapter II-Modem and an S7-200 controller
    4.3 Direct connection between a TS Adapter II-Modem and an S7-200 controller and a panel via MPI
    4.4 Direct connection between a TS Adapter II-Modem and an S7-200 controller, an S7-300 controller and a panel via MPI

Attachment 1: S7-200_WinCCflexRT_Panels.pdf ( 1107 KB )

Important
This entry contains information for editing the registry. You should make a backup copy of the registry before editing it. More information on making a backup copy, restoring and editing the registry is available in the Microsoft Knowledge Base in Entry ID 256986. Incorrect use of the registry editor can cause serious problems that affect the complete system and make it necessary to reinstall the operating system. You use the registry editor at your own risk.

Keywords:
COM port; COM interface, serial interface, Micro Automation, HMI

 Entry ID:28263099   Date:2010-02-09