show the entry list
S7-300 CPU 31x -- Product information -- Background and system information
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when using the alarm numbering procedure?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
What is the maximum number of parameters that can be assigned to an FC and FB in the S7-300 CPU?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Why is only a warm start available for S7-300?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which entries deal with consistent data in conjunction with distributed I/O?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
What are the requirements for using the S7 routing function and which modules can you implement?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Status of the run-time meter after overall reset
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Local data addressing with S7-300 / S7 400
S7 300 run-time meter doesn't give any value
Status of the run-time meter after overall reset
Part number:

QUESTION:
Is the run-time meter reset after an overall reset of the CPU?

ANSWER:
In the S7-300 and C7 complete devices a difference is made between CPUs with a hardware clock (integrated "real-time clock") and CPUs with a software clock. The last run-time meter value in the CPUs with a software clock with no back-up is deleted after an overall reset of the CPU. In the case of the CPUs with a hardware clock with back-up, the last run-time meter value is retained after an overall reset of the CPU.

Table 1 lists the CPUs with software clock. All other S7-300 CPUs and C7 complete devices have a hardware clock. The S7-400 CPUs all have hardware clocks.

CPU

Order no.

Run-time meter value is deleted/retained

CPU 312-IFM

6ES7 312-5AC0x-0AB0

No run-time meter

CPU 313

6ES7 313-1AD0x-0AB0

Deleted

CPU312

6ES7 312-1AD10-0AB0

Deleted

CPU312C

6ES7 312-5BD0x-0AB0

Deleted

C7-621

6ES7 621-1AD0x-0AE3

Deleted

C7-621 ASi

6ES7 621-6BD0x-0AE3

Deleted

Table 1: S7-300 CPUs and C7 complete devices with software clock


 Entry ID:2804630   Date:2003-11-05 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour