show the entry list
Touch Panel / Operator Panel -- Creating HMI configurations -- Tips and tricks for configuring
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
Button as pure illuminated indicator with a TP170A
Height of a textbox in a standard configuration (ProTool V6.0)
CPU functions for S7-300 with OP7/OP17
Picture change on the TP170A as tag function
"Tahoma" is the only font that can be used with OP/TP 170A/B and C7-635
How can you implement an OP73 as a handheld?
How can you implement an OP73 as a handheld?
Part number:

Instructions:
You can use the OP 73 as a handheld as follows:
Use a TD-PPI cable (6ES7 901-3EB10-0XA0) to connect the OP 73 directly to the MPI interface of an S7-300/400 controller or to the PPI interface of an S7-200 controller. You do not need an additional power supply for the OP.

Please pay attention to the degree of protection of the OP 73. The OP 73 has IP65 at the front and IP20 at the back.

The example below shows how you can configure an OP 73 as a handheld.
A sample project with the functions described is available for downloading at the end of this entry.
 
No. Procedure
1


Fig. 01

In "Picture 01" (Start picture) you enter the connection parameters for the communication connection of the OP73 to CPU.

Press the "Start" button or function key "F4" to execute the "Change Connection" function.
The "Change Connection" function disconnects the connection to the controller currently being used and sets up a new connection to the controller specified.

Use the "Up" and "Down" arrow keys to navigate to the individual IO fields. When the edge of the screen is reached, the page changes to the next picture.

2


Fig. 02

The following functions can be executed via Picture 02.

  • "F1" button - Terminate Runtime
  • "F4" button - Switch language (German/English)

Use the "Up" and "Down" arrow keys to navigate to the next picture.

3


Fig. 03

Figure 03 shows an example of how to output the value of one single DB.
In the "DB number" IO field you enter the relevant number of the data block, e.g. "10".
In the "Data word" IO field you enter the relevant number of the data word, e.g. "2".

In middle IO field you then get the content of "DB10.DBW2" displayed.
(You can also specify a value yourself in this IO field).

If the specified data block is not available in the controller, the system message "PLC address error" is displayed.

You can manually specify the IO addresses via function keys "F1" to "F4".

  • "F1": count up DB number step by step.
  • "F2": count down DB number step by step.
  • "F3": count up data word number step by step.
  • "F4": count down data word number step by step.

Use the arrow keys to navigate to the individual IO fields.
When the edge of the screen is reached, the page changes to the next picture.

4


Fig. 04

Figure 04 shows an example of how to output the values of two DBs.
In the "DB" IO field you enter the relevant number of the data block, e.g. "20".
In the "DBW" IO field you enter the relevant number of the data word, e.g. "2".
In adjacent IO fields you then get the content of "DB20.DBW2" displayed.
(You can also specify a value yourself in this IO field). Use the arrow keys to navigate to the individual IO fields.
When the edge of the screen is reached, the page changes to the next picture.

5 The following figure shows an online view of "Picture 04".


Fig. 05

Detailed information on configuring is available in the attached project.
The attached download contains the archived STEP 7 project and integrated WinCC flexible project.

  Attachment 1: Project_01.zip ( 3329 KB )

Runnability and test environment:
The example can be used on all the CPU types of SIMATIC S7-300 and S7-400.
The following table lists the components that have been used to create this entry and verify the functions described.
 
Components Product and version designation
PC operating system Microsoft Windows XP SP2
Standard tools STEP 7 V5.4 SP3
Engineering tools -
HMI software WinCC flexible 2007
HMI devices OP 73
Controllers S7 CPU 315-2DP
Table 1: Creation environment of the download attached

Keywords:
PDA, PDAs

 Entry ID:27879455   Date:2008-02-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour