|
Problem If a hydraulic axis is to be operated through the control loop of the technology CPU you need a compensation characteristic for optimal control., which maps the linear actuating signal of the controller onto the non-linear behavior of the hydraulic axis.
Solution
The technology template can be directly used for the measurement of the compensation characteristic of a hydraulic axis and for the activation of this characteristic in the control loop of the technology CPU.
Downloads
| Content of Downloads |
Download |
| Documentation |
 |
|
Code
The S7 Code of the Template Move3D can be downloaded separated or together with a example
For the Examples a
- CPU 31xT-2 DP
- IM174
- STEP 7 V5.5 SP2
- S7 Technology V4.2 SP1 and
- WinCC flexibel 2008 SP3 Runtime
are required. |
Program archive |
 |
| Program archiv with example for CPU 315T |
 |
| Program archiv with example for CPU 317T |
 |
History
| Version |
Modification |
| 11/2008 |
first edition |
| 03/2009 |
V4.11: Code correction of cam disc generation in point (0,0) |
| 05/2012 |
V4.2.1: Code correction initialization "MC_Halt" / Additional functions |
|