Instructions: The PS (power supply) expansion board is engineered in such a way that power is supplied either through the internal PC supply unit or the external supply. In the Box PC 627 there is a plug for the PS expansion board for connecting the internal power supply. The following table describes how you can connect the PS expansion board of the CPU 41x-2 PCI V3.4 (WinAC Slot) to the internal power supply of the Box PC 627:
| No. |
Procedure |
| 1 |
Loosen the two screws on the rear of the Box PC 627 and remove the top. |
| 2 |
Plug the 12V power cable supplied into the connector indicated in the Box PC 627.
 ( 105 KB )
Fig. 01
|
| 3 |
Connect the other end of the 12V power supply cable to the X1 connector on the PS expansion board.
 ( 108 KB )
Fig. 02 |
| 4 |
Close the PC box again and tighten the screws. |
Note: This description is also valid for the Panel PC 677, because the computer unit in the Panel PC is based on the same motherboard.
Keywords: WinAC Slot (Windows Automation Center), PLC CPU 412-2 PCI Slot , PLC CPU 416-2PCI Slot
|