|
QUESTION:
What is the load current of the enabling contacts at Ue > 24V and utilization category DC-13 for the 3TK2826 Safety Relays?
ANSWER:
For the 3TK2826 Safety Relays enabling contacts the following values are valid according utilization category DC-13:
Ue = 125 V: 0,2A
Ue = 250 V: 0,1A
These values are according EN 60947-5-1:1997 + A11:1997; appendix A according UL508, Rating Code R300, tested and official confirmed.
|