Operator panels for hazardous areas with potentially explosive atmosphere An overview of which operator panels you can use in hazardous areas with potentially explosive atmosphere is available in Entry ID: 291285.
Note More information about the range of functions of the SIMATIC HMI operator panels is available in the Online Help of WinCC flexible and WinCC (TIA Portal). A configurator for easy selection of SIMATIC HMI operator panels is available in the Industry Mall.
Keywords
Smart devices, WinCC, Windows Mobile, Operating system, OS, Pictures, Tags, Analog messages, Bit messages, Recipes, Tag archives, Message archives, Audit, Audit Trail, Scripts, Logs, Text list, Graphics list, User administration, Faceplates, ProAgent, WinAC MP, Buttons, Graphics display, IO field, Switches, Bar display, Performance features, Function features, Operator panel overview, System limits, Slider, Smart, Sm@rt, Server, Sm@rt server, Sm@rt client, HTML browser, User display, Internet Explorer, Pointer instrument, Trend display, Symbol library, Recipe display, Alarm display, Message window, Alarm indicator, flexible, WinCC flexible, Function, Functions, Elements, Comparison, CPU, Diagram, Properties, Technical data, Basic, Comfort, TIA Portal, Diagnosis display, Safety, Number of connections, 15363798
Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?
Configuration Notes:
You can connect a SIMATIC S7-200 CPU with different types of HMI devices. Here you must take into account differences in communications protocols, baud rates and the number of connections possible. The HMI device always plays the active part in the communication. This entry covers the following two aspects:
One HMI component with multiple SIMATIC S7-200 CPUs
Below is an overview of HMI components that can be connected with the SIMATIC S7-200. In the following table "Number of S7-200s" stands for the maximum number of S7-200 controllers that can be parameterized with the configuration tool. Unless otherwise marked in the table the maximum baud rate is
187.5 Kbit/s with PPI protocol
12.0 Mbit/s with MPI protocol
HMI components
Configuration tool1)
Number of S7-200swith
PPI protocol
Number of S7-200swith
MPI protocol
S7-200 via CP243-1
Ethernet
PP 7
Configuration tool not required
-
1 (max. 1.5 Mbit/s)
-
PP 17-I
Configuration tool not required
-
1 (max. 1.5 Mbit/s)
-
PP 17-II
Configuration tool not required
-
1 (max. 1.5 Mbit/s)
-
TD 17
As from ProTool / Lite V2.51
4
4
-
OP 3
As from ProTool / Lite V2.51
2
2 5)
-
OP 5
As from ProTool / Lite V1.01
4
2 5)
-
OP 7
As from ProTool / Lite V2.5
4
4
-
OP 15
As from ProTool / Lite V1.01
4
4 5)
-
OP 17
As from ProTool / Lite V2.5
4
4
-
OP 25
As from ProTool V1.31
4
4 (max. 1.5 Mbit/s)
-
OP 27
As from ProTool V3.1
4
4
-
OP 35
As from ProTool V1.31
6
6 (max. 1.5 Mbit/s)
-
OP 37
As from ProTool / Lite V2.5
8
8
-
TP 27
As from ProTool V3.1
4
4
-
TP 37
As from ProTool V3.1
8
8
-
TP 070
As from TP Designer version V1
-
1 (max. 19.2 Kbit/s)
-
OP 73 Micro
As from WinCC flexible 2004 Micro SP1+HSP1.1
1
1 (max. 187.5 Kbit/s) 2)
-
TP 170micro
As from WinCC flexible 2004 Micro
1
1 (max.187.5 Kbit/s)
-
TP 177micro
As from WinCC flexible 2004 Micro SP1+HSP1.1
1
1 (max. 187.5 Kbit/s) 2)
-
Mobile Panel 170
As from ProTool / Lite V6.0 SP 2, WinCC flexible 2004 Compact
1
4
-
Mobile Panel 177 DP
As from WinCC flexible 2005 Compact
1
4
-
Mobile Panel 177 PN
As from WinCC flexible 2005 Compact
-
-
4 4)
Mobile Panel 277
As from WinCC flexible 2005 SP1 Standard
1
8
8 4)
OP 73
As from WinCC flexible 2004 Compact SP1+HSP1.1
1
2 (max. 1.5 Mbit/s) 2)
-
OP 77A
As from WinCC flexible 2004 Compact SP1+HSP1.1
1
4 (max. 1.5 Mbit/s) 2)
-
OP 77B
As from WinCC flexible 2004 Compact
1
4
-
TP 170A
As from ProTool V6.0
1
1 (max. 1.5 Mbit/s)
-
TP 170A
As from WinCC flexible 2004 Compact
1
4 (max. 1.5 Mbit/s)
-
TP 177A
As from WinCC flexible 2004 Compact SP1+HSP1.1
1
4 (max. 1.5 Mbit/s) 2)
-
TP 170B
As from ProTool V6.0, WinCC flexible 2004 Compact
1
4
-
TP 177B 4" PN/DP COLOR
As from WinCC flexible 2008 Compact
1
4
4 4)
TP 177B DP
As from WinCC flexible 2005 Compact
1
4
-
TP 177B PN/DP
As from WinCC flexible 2005 Compact
1
4
4 4)
OP 170B
As from ProTool / Lite V5.2 SP 2, WinCC flexible 2004 Compact
1
4
-
OP 177B DP
As from WinCC flexible 2005 Compact
1
4
-
OP 177B PN/DP
As from WinCC flexible 2005 Compact
1
4
4 4)
TP 270, OP 270
As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard
1
8
8 4)
TP 277, OP 277
As from WinCC flexible 2005 Standard SP1
1
8
8 4)
MP 177
As from WinCC flexible 2008 Standard
1
8
8 4)
MP 270
As from ProTool V6.0
1
8
8 4)
MP 270B
As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard
1
8
8 4)
MP 277
As from WinCC flexible 2005 Standard SP1
1
8
8 4)
MP 370 Key
As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard
1
8
8 4)
MP 370 Touch
As from ProTool V6.0 SP 2, WinCC flexible 2004 Standard
1
8
8 4)
MP 377
As WinCC flexible 2005 Standard SP1
1
8
8 4)
PC IL 70
ProTool/Pro CS, WinCC flexible Advanced
1
8 (max. 187.5 Kbit/s)
8 4)
PC IL 77, PC 477,
PC 577, PC 670,
PC 677, PC 870,
PC 877
The required tool specified, if specified separately, is the minimum requirement with regard to release, version, service pack or HSP on the one hand and the tool version "Lite", "Compact", "Standard", etc. on the other hand.
2)
The HMI device can also communicate with an PPI master in the same network, if only S7-200 connections are configured in the project for it. This is the exception. An MPI master cannot usually access a PPI master in the same network.
3)
TD 200: the text display sets itself automatically to the protocol concerned.
4)
Only one HMI component can communicate with the S7-200 at any one time (on account of the connection management via TSAP).
5)
As from ProTool/Lite 3.0 and ProTool 3.0 you can also select the MPI and PROFIBUS protocol for OP3, OP5, OP15A and OP15C.
Note:
An MPI master cannot usually access a PPI master in the same network.
One SIMATIC S7-200 CPU with multiple HMI components Communication can be via the MPI or PPI protocol.
In the case of the MPI protocol the CPU communicates with each HMI device via a separate connection. This effectively avoids communication problems. However, the number of HMI devices that you can connect to an S7-200 CPU is greatly limited and depends on the type of CPU. The following table gives an overview.
MPI (DP/T)
Number of HMI comp.
CPU Port 0
Max. baud rate
CPU Port 0
Number of HMI comp.
CPU Port 1
Max. baud rate
CPU Port 1
Number of HMI comp.
EM 277 Port
CPU 212
(as from firmware 1.1)
3
19.2 kbit/s
-
-
-
CPU 214
(as from firmware 1.1)
3
19.2 kbit/s
-
-
-
CPU 215
3
19.2 kbit/s
5
12 Mbit/s
-
CPU 216
3
19.2 kbit/s
3
19.2 kbit/s
-
CPU 221
3
187.5 kbit/s
-
-
-
CPU 222
3
187.5 kbit/s
-
-
-
CPU 224
3
187.5 kbit/s
-
-
-
CPU 224XP
3
187.5 kbit/s
3
187.5 kbit/s
CPU 226
3
187.5 kbit/s
3
187.5 kbit/s
-
EM 277
-
-
-
-
5 /
max.12 Mbit/s
Special case: You can connect up to 3 pushbutton panels of the same type (PP7, PP 17-I or PP 17-II); these then all have the same functionality. You assign parameters to the pushbutton panels via the data block of the controller. S7-200 has only one data block and therefore multiple functions cannot be provided for the panels (Entry ID: 691006).
Note: Only one TP 070 without any other nodes may be connected to each CPU interface.
In the case of the PPI protocol, you can theoretically connect 32 nodes, that is a maximum of 32 HMI devices. However, with PPI in one time interval there is only ever one logical connection between the nodes (time multiplex), which is established and disconnected for each communication. The baud rate is max. 187 kbit/s. This practically reduces the number of HMI devices to three per interface.
Now, in PPI mode, if several HMI devices (PPI masters) access the CPU (PPI slave), it might happen that an HMI device constantly arrives at the CPU that is occupied by another HMI device (or by another PPI master) and is no longer updated. In this case, you should increase the update cycles of the HMI devices. You do this in the relevant configuration tools of the HMI devices or with the text displays TD 100/200(C) in the Micro/WIN text display wizard.
Use Advanced PPI if the master concerned supports it. This type of protocol uses a separate connection like MPI. For example, when setting the PG/PC interface in Micro/WIN, you can select Advanced PPI when choosing a PPI connection.
More information on communication protocols of the S7-200 is available in the "S7-200 System Manual", chapter 7 - Communicating over a Network, in Entry ID: 1109582 .
Why do you get a warning when generating the block FB163, F_FB_RNG_16 and why cannot you load the block when using the Mobile Panel 277F IWLAN and an S7 CPU 315F (with PROFINET)?
The FB163, F_FB_RNG_16 cannot be used for the PROFINET CPUs listed below. It exceeds the maximum permissible block size. The following warning is issued when the block is generated:
"The F block FB163 or the associated automatically generated F block exceeds the maximum size supported by the F CPU configured."
You can only use the FB162, F_FB_RNG_4 with S7 PROFINET CPUs 315F and the following order numbers. Up to four Mobile Panels 277F IWLAN can be used it.
6ES7315-2FH10-0AB0, CPU315F-2 PN/DP, 192KB
6ES7315-2FH13-0AB0, CPU315F-2 PN/DP, 256 KB
Keywords: Effective range
What support does Siemens AG offer to make products comply with FDA regulations?
The FDA is the USA authority for licensing drugs and is under the Ministry of Health. The FDA was founded in 1927 with headquarters in Rockville (Maryland).
The FDA's task is to protect public health in the USA. It regulates the safety and effectiveness of human and animal pharmaceuticals, biological products, medical products, food and radiating devices. The regulations apply to products produced in the USA and imported products.
The FDA is comparable in Germany with the TÜV and Ministry of Health.
Important regulation for Siemens AG products On August 20, 1997, the FDA's rule 21 CFR Part 11 on electronic records and signatures came into force. 21 CFR Part 11 (in brief: Part 11) defines the acceptance criteria of the FDA for the use of electronic records and signatures instead of drawings in paper form and handwritten signatures on paper.
Further information More information on the topic of GMP (Good Manufacturing Practice) is available at the following link: http://www.automation.siemens.com/pharma