show the entry list
Mobile Panels -- Product information -- Technical data and ordering information
Wich protective films can I use with SIMATIC HMI panels?
Where are the current declarations of conformity to be found for SIMATIC HMI panels (CE, UL, cUL, GOST)?
What should you watch out for when connecting the equipotential bonding to the connection box of a mobile panel?
How can you determine the "E-Stand" (hardware release) of an operator panel?
What is the power consumption or power dissipation of the SIMATIC HMI operator panels?
Which PROFINET services are supported by SIMATIC panels.
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
Which panels are certified for shipbuilding?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Which installation guidelines do you have to watch out for with the transponders for the Mobile Panel 227 IWLAN and the Mobile Panel 277F IWLAN?
Mobile Panel 170 can only be used with the connection box
Which Siemens department holds the EC conformity declarations for SIMATIC HMI?
Which SIMATIC Panels have the CCC certificate?
Which SIMATIC panels have or need an FCC certificate?
No yellow-red emergency stop switch on the Mobile Panel 170
No standard project in WinCE devices
S7 Distributed Safety -- Product information -- Technical data
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Why does my F system go into STOP at startup?
F Technology CPU 300/400 -- Product information -- Technical data
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Why does my F system go into STOP at startup?
Which values can you use with F CPUs and products of the ET 200 family for PFD, PFH and the proof test interval?
Which fail-safe signal modules of the distributed I/O can be combined with which fail-safe controllers?
Which hardware and software components are required to set up and operate an F system with SIMATIC S7-300F?
WinAC RTX -- Product information -- Determining performance and quantity frameworks
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Why does the Windows application load increase to 100% after installing WinAC RTX 2008/2009?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Part number:

Description
You can use the Excel table "S7fcotia.xls" for calculating monitoring and response times in a safety-related application with S7 Distributed Safety. The table is available for free downloading in Entry ID: 25412441.

The "S7fcotia.xls" table has three tabs. The first tab contains the calculation of the maximum runtime of the F runtime group depending on the F CPU used. Here, among other things, you enter the number of F function blocks used from the S7 Distributed Safety library.

The associated F function blocks are not provided in the "S7fcotia.xls" table for the Mobile Panel 277F IWLAN.

Max. response times of Mobile Panel 277F IWLAN 
 
  Time in ms
TRES_no_Fault
(max. response time without error)
25
TRES_one_Fault
(max. response time with one error)
25
Table 01

The following table shows how to incorporate the execution times of the F function blocks and incorporation of the maximum response time of the Mobile Panel 277F IWLAN in the "S7fcotia.xls" table.
 
No. Procedure
1 Determining the execution times of the F function blocks for Mobile Panel 277F IWLAN   
  1. Insert the number of used F programm blocks in the table at the attachment 1.  
  2. Note the automatically caluted values from your used F programm blocks.
2 Incorporating execution times in the "S7fcotia.xls" table
  1. Open the "S7fcotia" table and select the tab
    "Max. runtime of F runtime group".
  2. Manually enter the time value determined (from 1) in the "Sum of execution times" line (section "F-FBs/F-FCs from other F library") under the corresponding CPU in the "S7fcotia.xls" table.
  3. The "Max. runtime of F runtime group" section of the "S7fcotia.xls" table displays the sum of the execution times of the F runtime group.

Then continue with "Estimation of the automation system's response time".

3 Incorporating maximum response times in the "S7fcotia.xls" table
  1. Open the "S7fcotia" table and select the tab
    "Max. response times".
  2. The "Observed signal flow of the safety function" section lists four different F I/O versions.
    Select the version corresponding to your system configuration and enter the maximum response time (see Table 01) in the cells provided (TWCDT and TOFDT).

Then continue with "Estimation of the automation system's response time".

Instructions for this are available in Entry ID: 23926783.

Table 02

Excel table "27097159_Runtime_F_FB_V1_1_en.xls"
The attached Excel table "27097159_Runtime_F_FB_V1_1_en.xls" is for easy addition of the execution times of the F program blocks for the Mobile Panel 277F IWLAN.
Enter the time value determined in the "Sum of execution times" line (section "F-FBs/F-FCs from other F library") in the "S7fcotia.xls" table.

Attachment 1: Runtime_F_FB_V1_1_en.xls ( 28 KB )  

 Entry ID:27097159   Date:2011-10-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour