show the entry list

ET 200pro -- Product information -- Technical data 
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm? 
Which CPU can you operate as a PROFINET I device? 
What are the requirements for using the S7 routing function and which modules can you implement? 
What is the significance of the IP protection classes IP65, IP66, IP67? 

How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?Go to beginning
Part number:

Instructions
This value is dependent on the conversion time, the type of measurement (current, voltage and resistance measurement) and the number of active channels.

The total conversion time determined (basic conversion time + additional conversion times) for a channel has to be multiplied by the number of active channels. This gives you the cycle time for a module. A signal must be present for at least this time to ensure that it is recognized as a process alarm.

The following manuals give information on the length of the basic conversion times of the various modules and on any additional conversion times that might have to be taken into account 
 
Modules Manual

Entry ID

ET200M  SIMATIC S7-300 programmable logic
controller, module data
8859629
ET200S  SIMATIC ET 200S distributed I/O system 
1144348
ET 200iSP SIMATIC ET 200iSP distributed I/O device 28930789
ET 200pro SIMATIC ET 200pro distributed IO system 21210852
ET 200eco PN SIMATIC ET 200eco PN distributed I/O device 29999018

If smoothing of the input signals has also been configured, the smoothing level which has been parameterized has to be taken into account. The smoothing levels (weak, medium and strong) are multiples of the cycle time and vary depending on the module used. 
The smoothing level attenuates the rise of an input signal. The specification in cycles indicates in how many cycles an input signal with 63% of its maximum value is recognized

Note
Refer to the manuals listed above to find out the number of cycles per smoothing level for your module.

Which CPU can you operate as a PROFINET I device?Go to beginning
Part number:

Description
You can operate an ET200 CPU or an S7 CPU as PROFINET I device (intelligent IO device). The following holds here:

  • An S7-300 CPU can be used as an I device as from firmware version V3.2.0.
  • An S7-400 CPU can be used as an I device as from firmware version V6.0.0.
  • An ET200S or an ET200pro CPU can be used as an I device as from firmware version V3.2.0.
  • You need at least STEP 7 V5.5 for the configuration.

Note
More information about the PROFINET I-device function is available in the system manual "PROFINET, System Description" in the chapter entitled "I Device" in Entry ID 19292127.

What are the requirements for using the S7 routing function and which modules can you implement?Go to beginning
Part number:

Description
From STEP 7 V5.0 SP3 HF3 onwards you can reach ST stations online over and beyond subnet limits with the PG/PC, in order, for example, to load user programs or a hardware configuration or in order to execute test and diagnostic functions. You can connect a PG/PC at any place within the network and connect online to any stations which are reached through gateways.

Gateway
The gateway from a subnet to one or more other subnets is in a SIMATIC station that has interfaces to the subnets concerned.

Requirements

  • At least STEP 7 V5.0 SP3 HF3 is installed on the PG/PC for configuration and use of the S7 routing function.
  • An interface (Industrial Ethernet or PROFIBUS PC CP) is installed in the PG/PC to establish a connection to the gateway. You can use PROFIBUS PC CPs 55xx and 56xx. You can use any NDIS-compatible Ethernet network card (3COM, CP1613, for example) as Industrial Ethernet interface in the PG/PC.
  • The associated communications modules of the station support the S7 routing function.
  • The network configuration does not go across project boundaries.
  • Both the modules and the PG or PC are loaded with the configuration information that contains the latest "knowledge" about the complete network configuration of the project.
    Technical background
    All the modules associated with the gateway must receive information about which subnets can be reached over which routes (= routing information).

Note
The lists below have been updated with the modules of the hardware catalog of STEP 7 V5.4 SP2. This means that older modules which support the S7 routing function are listed in the tables, but are not necessarily included in the hardware catalog of the latest versions of STEP 7.

SIMATIC S7-CPUs
The list below gives an overview of the SIMATIC S7 CPUs that support the S7 Routing function.

584459_Overview_CPUs_en.pdf ( 43 KB )

Communications processors (CPs)
The list below gives an overview of the PROFIBUS and Industrial Ethernet CPs that support the S7 Routing function.

584459_Overview_CPs_en.pdf ( 41 KB )

SIMATIC S7 FM modules
The list below gives an overview of the SIMATIC S7 FM modules that support the S7 Routing function.
 

FM

Version

Order number

FM 356-4 V5.0 V5.0 6ES7356-4BM00-0AE0
FM 356-4 V5.0 V5.0 6ES7356-4BN00-0AE0
FM 456-2 V5.0 6ES7456-2AA00-0AB0
Table 01

Gateways
The list below gives an overview of the gateways that support the S7 Routing function.
 

Link

Version

Order number

IE/PB Link as from V1.0 6GK1411-5AA00
IE/PB Link PNIO as from V1.0 6GK1411-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB01
Table 02

SIMATIC S7 IM modules
The list below gives an overview of the SIMATIC S7 IM modules that support the S7 Routing function.
 

IM

Version

Order number

IM 467 as of V2.0 6ES7467-5GJ02-0AB0
IM 467 FO as of V2.0 6ES7467-5FJ00-0AB0
Table 03

SIMATIC WinAC RTX, WinAC Slot and WinAC MP
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
WinAC Version Order number
WinAC RTX as from V4.0 6ES7671-0R...
WinAC Slot 412 as from V3.2 6ES7673-2C...
WinAC Slot 416 as from V3.2 6ES7673-6C...
WinAC MP as from V4.1 6ES7671-4EE00-0YA0
6ES7671-5EF01-0YA0
6ES7671-7EG01-0YA0
Table 04

SINAUT communications modules
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
TIM Version Order number
TIM 3V-IE as from V1.0 6NH7800-3BA00
TIM 3V-IE Advanced as from V1.1 6NH7800-3CA00
TIM 4R-IE as from V1.0 6NH7800-4BA00
TIM 4RD as from V3.x 6NH7 800-4AD90
Table 05

Note
The target station does not have to support the S7 Routing function.

Additional Keywords
Module function

What is the significance of the IP protection classes IP65, IP66, IP67?Go to beginning
Part number:

Configuration Notes:
The protection rating indicates how suitable electrical equipment (e.g. devices, lighting, installation material) is for various environmental conditions and also the protection for people against potential dangers when using the equipment.

With regard to suitability for various environments, the systems are divided into relevant IP codes (Ingress Protection codes).

The protection rating is always indicated by the letters IP followed by two digits.
The first digit indicates the degree of protection against contact and solid foreign objects.
The table below explains the meanings of the first digits of the IP code.
 
Digit Protection against body contact Protection against solid foreign objects
0 No protection No protection
1 Protected against large parts of the body
(diameter 50mm)
Large solid foreign objects
(diameter 50mm and greater)
2 Finger protection
(diameter 12mm)
Medium-size solid foreign objects
(diameter 12.5mm and greater, and length up to 80mm)
3 Tools and wires
(diameter 2.5mm and greater)
Small solid foreign objects
(diameter 2.5mm and greater)
4 Tools, wire, and small wires
(diameter 1mm and greater)
Granular solid foreign objects
(diameter 1mm and greater)
5 (K) Wire protection (as IP4), dust-protected Dust deposit (not harmful)
6 (K) Wire protection (as IP4), dust-tight No ingress of dust

The second digit indicates the degree of protection against liquids.
The table below explains the meanings of the second digits of the IP code.
 
Digit Protection against liquids
0 No protection
1 Protected against vertically falling drops of water
2 Protected against direct sprays of water up to 15° from the vertical
3 Protected against direct sprays of water up to 60° from the vertical
4 Protected against water sprayed from all directions, limited ingress permitted
4k Protection against water sprayed from all directions under increased pressure, applies only to road vehicles
5 Protected against low pressure jets of water from all directions
6 Protected against heavy seas or powerful water jets (flooding)
6k Protected against powerful water jets under increased pressure (flooding), applies only to road vehicles
7 Protected against the effects of temporary immersion in water
8 Protected against the effects of continuous immersion in water
9k Protection against high-pressure/steam-jet cleaning, applies only to road vehicles

Note:
Each protection rating is to be considered separately. A high protection rating does not automatically include a lower protection rating.

 Entry ID:27089831   Date:2012-12-13 
I regard this article....as helpfulas not helpful                                 






























related links
Which modules can you use when im ...
What are the requirements for usi ...
SIMATIC S7-300 Instruction list S ...
What is multicomputing mode and w ...
How many communication instances ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour