show the entry list
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
ProTool -- Creating HMI configurations -- Loading and testing configurations
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
Transferring the ProTool/Pro Runtime file (*.fwd) from the configuration computer to the visualization PC with the ProTool/Pro RT Loader
Automatic reset to serial transfer mode when the project download in ProTool V6.0 SP1 failed
ProTool Lite - Error when transferring a project
How can you transfer a ProTool project via MPI/PROFIBUS to a Windows-based panel?
How is an OP3 connected for the serial transfer of the configuration to the configuration PC?
What is the pin assignment for the adapter cable 6XV1440 - 2DE32 (TTY/V24)?
What is the serial cable assignment for transferring the configuration to an RMOS operator panel?
How do you make an MPI cable extension for an OP3?
What is the pin assignment for the plug-in connecting cable TD/OP <-> CP521 SI (V24)?
What is the serial cable assignment for transferring the configuration to a Windows-based device?
How do you load a project onto the operator panel with ProTool?
How do you use ProTool/Pro to configure the communication between a Windows-based operator panel and an S7 station via routing?
Why is the connection interrupted while transferring a project with ProTool to an OP?
Why can you not transfer the configuration from the PC to the Windows CE-based panel?
Using serial ports as of COM3 for ProTool project transfer from the PC to the panel
Mobile Panels -- Creating HMI configurations -- Remote access - tips and tricks for configuring
How can you access tags of an operator panel using an Excel application with WinCC (TIA Portal)?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
How do you use a key switch to lock/activate the call of specific screens?
How do you temporarily lock multiple operator panels?
How can you access tags of an operator panel using an Excel application with WinCC flexible 2008?
Multi Panel -- Creating HMI configurations -- Remote access - tips and tricks for configuring
How can you access tags of an operator panel using an Excel application with WinCC (TIA Portal)?
OPC connection to a panel not possible with ProTool V6.0 SP1A
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
How do you use a key switch to lock/activate the call of specific screens?
How do you temporarily lock multiple operator panels?
How can you access tags of an operator panel using an Excel application with WinCC flexible 2008?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
Part number:

Using the TS Adapter IE:
Using the TS Adapter IE (TSA-IE), you can transfer the configuration of a panel or PC connected to an Ethernet network via the telephone network.


Fig. 01

Settings of the TS Adapter IE
The example below shows the settings to be made on the TS Adapter IE in order to transfer a configuration from your local computer to a panel or Runtime PC.
 
No. Procedure
1 Open "Options" dialog
For project transfer via the telephone network and the TS Adapter IE (TSA-IE) in an Ethernet network, you must parameterize the integrated firewall of the TS adapter.
  • Start the TeleService program.
  • In TeleService, you open the dialog "Options > Administrate TS Adapter IE...".


Fig. 02

2 Enable protocols
The relevant protocols for incoming and outgoing calls must be enabled. Below is an explanation of the settings required for incoming calls. The settings for outgoing calls are to be made in the same way.
  • Enable the necessary protocols for transfer in the firewall settings of the TS Adapter.
  • Click on the "Save settings" button.


Fig. 03

3 Enable ICMP
The ICMP (Internet Control Message Protocol) allows the TS Adapter IE to access IP addresses in the Ethernet network.
  • Switch to the "Internet protocols" tab.
  • Enable the ICMP protocol.
  • Click on the "Save settings" button.


Fig. 04

4 Configure port release
In Expert mode the ports via which the configuration is transferred must be allowed in the firewall of the TS Adapter. Normally, the transfer is via Port 2308 or alternatively via Port 50523.
  • Switch to the "Expert mode" tab.
  • Release Ports 2308 and 50523 in the settings mask.
    Note:
    If you have an active firewall, you must release the following ports as well for the Internet services given below:
     
    Internet service

    Port

    MiniWeb 80
    Remote Control via Internet Explorer 5800
    Remote Control via Sm@rtClient 5900

    Other ports used by WinCC flexible are listed in Entry ID 24534065.

  • Save the setting made before you quit the settings mask.


Fig. 05

5 Settings for the outgoing calls
  • Now make the aforementioned settings for the outgoing calls too.

    Finally, the firewall of the TS Adapter IE is configured so that a transfer can be made by ProTool or WinCC flexible.

Keywords:
Operator panel, Panel

 Entry ID:26999934   Date:2008-06-09