| Operation of the configuration
  Bild 02
Point 1:
Output of the current HMI time.
Point 2:
Output of the current PLC time.
Point 3:
Via the IO fields you can change the PLC time via the operator panel.
Use the "Set PLC Time" button to transfer the specified time to the PLC.
Point 4:
Graphics and text output indicating whether summer time or winter time is active.
Setting/presetting of summer/winter time
The central European states have Central European Summer Time, CEST, from the last Sunday of March to the last Sunday of October, at 2 a.m. central European time in each case.
Setting the summer time Points 5/6:
Here you can specify the following, for example: "last", "Sunday". Alternatively you can specify any other date (e.g. "1st", "Monday" etc.).
If you wish to specify a fixed day, select ">Day<" via Point 6. You can then specify the weekday under Point 5.
Point 7:
Specification of the month.
Point 8:
Specification of the time when summer time begins.
Setting the winter time Point 9:
In this area you specify when winter time is to begin.
The procedure is the same as for the summer time. |