show the entry list
PROFIBUS S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you program the communication blocks FC50 and FC60?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Mode blocks are already being used in the user program?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for using the PROFIBUS DP protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the free Layer 2 of the FDL protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol?
Where can you find sample programs and documentation for using the PROFIBUS FMS protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules as well as for data communication between SIMATIC S5 modules and PCs?
Notes on using an instance for multiple connection IDs
Processing the data from DP slaves via CP342-5 on CPU31x
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
How do you program the communication blocks FC5 and FC6?
What properties and special features does S7 Basis Communication offer?
PROFIBUS: diagnostics of S7 connections with STEP 7
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
Particularities when assigning parameters of the communication blocks of CP 342 / CP 343
What should you watch out for when upgrading the CP 342-5 or fitting spare parts?
Which version of the function blocks do you need to operate a CP 342-5?
CP 342-5 -- How can you tell that the CP 342-5 has withdrawn from the PROFIBUS?
CP 342-5 -- How do you program data communications when your DP slave only has outputs?
CP 342-5 -- How can you read and write consistent data of a DP slave via the CP 342-5?
What properties and special features does S7 Basis Communication offer?
Part number:

Configuration Notes:
All recent (not high-availability) S7/M7 300/400s (incl. WinAC Slot 41x) and C7-600 CPUs have simple functions (SFCs) for transferring small volumes of data via S7 connections. The connections are not configured, but are set up explicitly when the SFC is called and transfer the data either via the MPI bus or via PROFIBUS DP.

Like S7 communication, S7 basic communication also uses the S7 protocol for data transfer. The S7 protocol is on Layer 7 (Application Layer) of the ISO-OSI reference model, because the system interface used is purely for application data.

( 46 KB )
Fig. 01: ISO-OSI reference model

Protocol services:
 
Type of service Description
I_PUT / I_GET Permits reading / writing of data of an I slave on the PROFIBUS DP.
X_PUT / X_GET Permits reading / writing of data of another MPI or backplane bus node.

Note:

  • A detailed description of the I and X functions is available in the sample application "Communication with SIMATIC S7", section 3.1.2 in Entry ID: 20982954.
  • An example of "Client / Server Communication with (I) Slaves via S7 Basic Communication (I_PUT/ I_GET)" is available in Entry ID: 20987910.

Keywords:
Not configured connection, X_SEND, X_RCV

 Entry ID:26701842   Date:2007-10-31 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour