show the entry list
Sales and delivery release for the innovated SIMATIC ET 200S FC
Part number:
Summary Internet document

The new generation of the SIMATIC ET 200S FC frequency converter is now released for general availability.

The frequency converter offers the main new functions:

  • The frequency converter can be controlled (open-loop) via Profidrive 4.0 interface with standard telegram 1
  • The frequency converter can be parameterized using the Starter PC-based tool via a fieldbus

Internet document Summary

Update dd. June 10, 2011

New functions

The innovated ET 200S FC frequency converter will be released with Firmware V3.0, the firmware platform of the SINAMICS G120. In addition to all of the improved functions - that have been incorporated in this firmware within the scope of the ongoing development of SINAMICS G120 - for SIMATIC ET 200S FC, three essential new functions are now available:

  • The SIMATIC ET 200S FC frequency converter, as well as also the SINAMICS G120, will be addressed from the higher-level control via the Profidrive 4.0 profile. Standard telegram 1 was implemented in ET 200S FC. It is no longer necessary to use the FB100 communication block - that was previously required; this has now been completely eliminated.
  • The parameters in the frequency converter can be read and written to using a data set (DS47), the non-cyclic data set communication from Profidrive 4.0. For this, the DPV1 mode must be provided in the Interface Module IM151 for PROFIBUS!
  • The frequency converter can be parameterized using the Starter PC-based tool via a fieldbus. The possibility of using this "routing" via the station header depends on the IM151 interface module that is being used, which must be operated in the DPV1 mode. In general, "Routing" is not supported via the Profibus CPU station headers.

Ordering information

The control modules and the power units can be ordered by specifying the following Order Nos. [MLFBs]:
Order No. Description
6SL3244-0SA00-1AA1 Control module ICU24
6SL3244-0SA01-1AA1 Control module ICU24F
6SL3225-0SE17-5UA1 Power unit IPM25 750 W
6SL3225-0SE22-2UA1 Power unit IPM25 2.2 kW
6SL3225-0SE24-0UA1 Power unit IPM25 4.0 kW

The terminal modules of the ET 200S FC remain unchanged:
Order No. Description
3RK1903-3EA10 Terminal module for ICU24/ICU24F
3RK1903-3EC00 Terminal module for IPM25, 65mm, with power infeed
3RK1903-3EC10 Terminal module for IPM25, 65mm, without power infeed
3RK1903-3ED00 Terminal module for IPM25, 130mm, with power infeed
3RK1903-3ED10 Terminal module for IPM25, 130mm, without power infeed

The ET 200S FC options also remain unchanged:
Order No. Description
6SL3203-0BE22-5AA0 EMC filter, Class A, 25A (externally mounted)
6SL3203-0BE25-0AA0 EMC filter, Class A, 50A (externally mounted)
6SL3254-0AM00-0AA0 Memory card for parameterization (MMC format)
6ES7901-1BF00-0XA0 Cable for a point-to-point connection PC - ICU24

Compatibility with the IM151 interface module

The innovated ET 200S FC frequency converter has been released for operation with all the current Profibus interface modules. Routing via the ET 200S IM is only possible if the IM supports DPV1 services.
Order No. Description DPV1
6ES7151-1AA04-0AB0 Interface module IM151-1 Standard yes
6ES7151-1BA02-0AB0 Interface module IM151-1 High Feature yes
6ES7151-1AB02-0AB0 Interface module IM151-1 FO for fiber cable no
6ES7151-1AB05-0AB0 Interface module IM151-1 FO for fiber cable yes
6ES7151-1CA00-3BL0 Interface module IM151-1 Compact, 16DI/16DO no
6ES7151-1CA00-0AB0 Interface module IM151-1 Basic no
6ES7151-1CA00-1BL0 Interface module IM151-1 Compact, 32DI no

The innovated ET 200S FC frequency converter has been released for operation with all the current Profibus interface modules with integrated CPU (the routing functionality is not provided when using CPU station headers):
Order No. Description
6ES7151-7FA20-0AB0 IM151-7 CPU be carried out
6ES7151-7AA00-0AB0 IM151-7 CPU, 24 kB
6ES7151-7AA10-0AB0 IM151-7 CPU, 48 kB
6ES7151-7AA11-0AB0 IM151-7 CPU, 64 kB
6ES7151-7AA13-0AB0 IM151-7 CPU, 64 kB
6ES7151-7FA20-0AB0 IM151-7 F-CPU
6ES7151-7FA01-0AB0 IM151-7 F-CPU
6ES7151-7FA00-0AB0 IM151-7 F-CPU
6ES7151-7AB00-0AB0 IM151-7 CPU FO with fiber cable interface

 
Order No. Description
6ES7151-3AA22-0AB0 Interface module IM151-3 PN Standard
6ES7151-3BA22-0AB0 Interface module IM151-3 PN High Feature
6ES7151-3BB22-0AB0 Interface module IM151-3 PN FO with fiber cable cable interface

The routing functionality is always provided when using the PROFINET IM151 station headers.

Compatibility with the previous device

The innovated SIMATIC ET 200S FC frequency converter mechanically fits on the same terminal module; however, beyond this it is not compatible with its predecessor.
  New control modules
6SL3244-0SA00-1AA1
6SL3244-0SA01-1AA1
Old control modules
6SL3244-0SA00-1AA0
6SL3244-0SA01-1AA0
New power units
6SL3225-0SE17-5UA3
6SL3225-0SE22-2UA3
6SL3225-0SE24-0UA3
Permissible Not permissible
Old power units
6SL3225-0SE17-5UA2
6SL3225-0SE22-2UA2
6SL3225-0SE24-0UA2
Not permissible Permissible

Table 1: Combination of control modules and power units

According to Table 1

  • The new control modules cannot be operated together with the "old" power unit.
  • The "old" control modules cannot be operated together with the new power unit.

More detailed information is provided in 40621110


zoom ( 231 KB )

Fig. 1: Non-compatible replacement of an ET 200S frequency converter

According to Fig. 1

  • When replacing "old by new" - the complete frequency converter must always be replaced - comprising control module and power unit.
  • After replacing "old by new" the ET 200S station in HW Config must be re-configured.
  • In addition, the control program must be adapted to the new communication interface (Profidrive instead of FB100)

The parameterization (parameter assignment) of an "old" frequency converter may not be downloaded into a new frequency converter; neither via the Starter PC-based tool nor via an MMC.

As result of this incompatibility, the ICU24/ICU24F 6SL3244-0SA0x-1AA0 control modules and the 6SL3225-0SExx-xUA2 power units are still available as spare parts.

Manuals

Starter commissioning tool

The ET 200S FC frequency converter will be commissioned using Starter V4.1. SP1 (or later). The Starter V4.1 SP2 is required for operation on PROFINET.

Information material

Configurators

 Entry ID:26556402   Date:2011-08-01 
I regard this article....as helpfulas not helpful                                 
related links
Operating Instructions: Frequency ...
Parameter Manual: ET 200S FC Cont ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour