Description If project texts and picture objects are displayed shifted on a PC Runtime station, this might be due to one of the causes below.
- "Normal size (96 DPI)" is set for the DPI setting on the configuration computer.
- The DPI setting is set to "Large size (120 DPI)" on the visualization PC on which PC Runtime is running.
The "Large size (120 DPI)" setting for the DPI setting on the visualization PC causes all the fonts in the project to be displayed enlarged. Thus the fields configured are too small for the character strings.
| Original with 96 DPI |
Enlarged with 120 DPI |
The example has been created, generated and displayed with 96 DPI.

Fig. 01
|
The example has been created and generated with 96 DPI, but enlarged through the operating system setting (120 DPI).

Fig. 02
|
The "Large size (120 DPI)" setting for the DPI setting can also cause shifting of the picture elements.
Note that you must always have the same DPI setting and the same font size set on the configuration PC and on the visualization PC on which PC Runtime is running.
Windows CE-based operator panels like the MP 277, for example, use the DPI setting "Normal size (96 DPI)".
The configurations should therefore be made on a configuration computer with the DPI setting "Normal size (96 DPI)" and font size "Normal".
Setting in the different Windows operating systems:
Windows 7
- Open the dialog: "Start > Control Panel > View: Small Symbols > Display".
- Here you select "Less than - 100% (standard)" and confirm with "Apply".
Note
If you want to check the actual DPI settings, click the link on the left: "Define user-defined font size (DPI)". The DPI value is output under the ruler.
The display is shifted in PC Runtime with Windows 7 only if the option "Use DPI scaling in Windows XP style" is active.
If you do not activate this option, the Runtime is scale linearly like a graph and is therefore displayed slightly out of focus. The display is not shifted.
WinXP
- Open the dialog: "Start > Settings > Control Panel > View > Tab: Settings > Button: Advanced > Tab: General".
- Under "Display" you select "Normal size (96 DPI)" for the DPI setting.

Fig. 03
- Now start the dialog: "Start > Settings > Control Panel > View > Tab: Appearance".
- Select "Normal" for the font size.

Fig. 04
Win2000
- Open the dialog: "Start > Settings > Control Panel > View > Tab: Settings > Button: Advanced > Tab: General".
- Under "Display" you select "Small Fonts" for the font size.

Fig. 05
Win98
- Open the dialog: "Start > Settings > Control Panel > View > Tab: Settings > Button: Advanced > Tab: General".
- Select the "Small Fonts" setting for the font size.
WinNT
- Open the dialog: "Start > Settings > Control Panel > View > Tab: Settings".
- Select the "Small Fonts" setting for the font size.
Keywords
Truncated, Incomplete, In part
|