show the entry list
ES - SIMATIC Manager -- Working with projects -- Compiling OS and loading OS
What should you watch out for when downloading from the WinCC/PCS 7 Engineering Station to the Operator Station (ES-OS download)?
Why aren't all the block icons updated during OS compilation?
Which settings should you check if OS loading fails with PCS 7 or the OS project cannot be activated?
Problems when mapping data blocks with the same name
How can you clear the following error message during OS compilation: "The number of parameters for the structured DM variables xxx of type yyy does not match the number of operator-controlled connections...".
What is the meaning of the error message "A structure conflict occurred when creating the structured DM variable XXXX of type YYYY..." when compiling the OS?
How do you set the TCP/IP protocol for PLC-OS data transfer?
What is the meaning of the warning in the log file "*** Warning(s) ***: The structure type XXXX has been changed since the last compilation. All associated structured tags (even other S7 programs) will be deleted on the OS." ?
How do you use the template pictures "@PCS7Typicals*.pdl" to create block icons?
What does the compile OS error message "302:3018 - There are process variables whose names are not unique within the project after replacing special characters..." mean?
Which messages may appear in the "Download OS" dialog box?
Why appears the error message "The number of external DM variables in WinCC exceeds the permitted in total number", although the necessary license is available?
With PCS 7, why can't you open the OS project on the OS after it is downloaded from the ES?
Which special characters/separators may not be used in PCS7 V4, V5, and how are they replaced during AS/OS transfer?
What are the requirements for performing an online delta loading of the OS?
Why does the automatic package update of the clients sometimes not work in case of a changes-only download?
What do you do if a text which is configured in the CFC appears different in runtime?
How is a text, which has been configured in the CFC, transferred into the OS during OS compilation, and what do you have to watch out for in particular during configuration?
Which work steps are necessary for a project update of a redundant server couple and the MultiClients in SIMATIC PCS 7 V5.x?
Which work steps are necessary for the update of the OS Runtime data for the migration from PCS 7 V5.x to SIMATIC PCS 7 V6.x?
What do you do in PCS 7 V7.0 if the OS compile process is interrupted because the WinCC project cannot be opened?
Why can WinCC tags have the status "write-protected" and thus cannot be edited, deleted or moved?
What has to be watched out for during the compilation of a modification into the OS-Station after the interface modification of a Function block?
Why can't you transfer the elements of an S7 structure or UDT to WinCC through OS compilation?
Why doesn't OS delta load from the SIMATIC PCS 7 ES work despite Runtime being active on the OS station?
Why do you get a warning to the effect that your OS project is running in demo mode when testing it on your ES?
How can you clear the error message "Download (310:88)"?
How can you correct the error message "OS is currently being loaded from another ES"?
How is server data (server package) generated and loaded?
After reloading the OS project to the server from the ES, how do you clear the undefined error message and the abort?
When compiling the OS project, how can you clear the internal error 15500 in the transfer.log file?
Why does the error message "FileCopyError ....WinCC6.0_Project\GraCS\Default.pdd" occur when making a delta load and what is the "Default.pdd" file for?
Why are texts no longer updated with PCS 7 V6.0 SP3 + SP3 Postfixes after an OS delta compilation and OS delta load?
How do you clear the error message "*** Error(s) ***: Error while requesting messages from the STEP 7 message server...."?
How do you clear the error message "Internal error: transfer of process variables has been aborted. Error number: 15424" when compiling the OS project?
How can you clear the error message "No DM variable can be created for a symbol without a name" during OS compilation?
Why can't you load a project via a network?
How is a text, which has been configured in the CFC, transferred into the OS during OS compilation, and what do you have to watch out for in particular during configuration?
Part number:

Instructions:
Different texts for a measuring point can be configured in the CFC which can be displayed in the process screen or in the alarm list in runtime.

The screenshots shown in this entry depict a scenario where "kg" is to appear as the unit for a measuring point in the process screen. The unit can be specified in the dialog box "Properties - Input/Outputs" in the CFC.


Fig. 01
 

Note:
The "Unit" entry field for a block I/O only appears if the I/O possesses the attribute "S7_unit". The attributes are allocated during the programming of a block, although they can also be allocated or modified afterwards. You can find notes on this in the PCS 7 Online Help under "Configuration - Engineering System > Implementing the PCS 7 Configuration > Creating the Master Data Library > Adapting Blocks > How to Modify Attributes of the Block I/Os".

During OS compilation, the texts are transferred from the CFC into the OS text library.


Fig. 02
 

Internal "text reference"-type tags are additionally created in the WinCC Tag Management during OS compilation for texts which appear in the process screen (e.g. unit, identifier or comment).


Fig. 03
 

These text reference-type tags contain the text ID of the Text Library as the starting value.


Fig. 04
 

The text reference-type tags are used to display Text Library texts in the screen.


Fig. 05
 


Fig. 06

It is advantageous to know the circumstances under which texts, which are configured in the CFC, are transferred to the OS Text Library.
 
No. Description
1 New entry in the OS Text Library
A new entry is only added to the Text Library during compilation if the text doesn't already exist in the library.

Attention
The following conditions govern internal decisions on whether or not texts already exist in the Text Library:

  • "Language for Display Devices"
    The check on whether or not a text already exists in the Text Library is performed in accordance with the default language for display devices selected in the SIMATIC Manager. You can call up the dialog box for specifying the default language for display devices in the SIMATIC Manager with the menu command "Options > Language for Display Devices...".
     
  • Upper/lower-case lettering is irrelevant
    Texts in the CFC which only differ from texts in the Text Library in terms of one, more or all of the letters in the texts are deemed to already exist. They are not inserted into the Text Library as new entries.
2 No new entry in the OS Text Library
If the requirements for the conditions described in line 1 are not met, two different scenarios may arise:
  • Change to an existing entry in the Text Library
    The existing entry in the Text Library is only changed for the default language for display devices set in the SIMATIC Manager. Should the text which is configured in the CFC only differ from an entry in the Text Library in terms of upper/lower-case lettering, a change is made.

    Note:
    The situation can arise where an existing text is changed in the Text Library during OS compilation. If the text was originally created using the OS Project Editor, the change is undone again the next time the OS Project Editor is run.
     
  • The Text Library is not changed
    The existing entry in the Text Library is not changed.

A number of factors dictate which of the two scenarios occur, e.g.

  • the order in which the relevant blocks have been inserted into the CFC
  • whether the OS compilation is performed in its entirety or in respect of changes.

Entry ID 26248773 describes how this can be affected directly.

 Entry ID:26249757   Date:2007-08-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour