|
DESCRIPTION
This contains the last two STARTER versions and additive SINAMICS Support Packages:Him
This contains version V4.3 SP2 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems. The download also contains the additive SINAMICS Support Packages in the file "Vol_2a_STARTER_V43_SP2_ SSPs_G110_G120.zip" and "Vol_2b_STARTER_V43_SP2_ SSPs_Family_Integrated":
- SSP SINAMICS V4.6
- SSP SINAMICS G120 V4.6
- SSP SINAMICS MV V4.6
These SSPs are automatically installed by the STARTER setup when the checkboxes are activated in the selection screen form.
SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key. However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Order number: 6SL3072-0AA00-0AG0.
STARTER V4.3 SP2 supports German, English, French, Spanish and Italian.
The following drive systems are supported (recently included versions compared to the previous STARTER V4.3.2 are marked in bold):
- MICROMASTER 4th generation
- SINAMICS DCM with firmware V1.1, V1.2, V1.3
- SIMATIC ET200S FC with firmware V1.0.x, V3.0.x
- SIMATIC ET200pro FC with firmware V3.0.x
- SINAMICS G110 with firmware V1.0.x, V1.1.x
- SINAMICS G110D with firmware V3.3.x, V3.4.x
- SINAMICS G120 with firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x, V4.2, V4.3.0, V4.3.2, V4.4, V4.5 and (with SSP) V4.6
- SINAMICS G120C with firmware V4.4, V4.5 and (with SSP) V4.6
- SINAMICS G120D with firmware V3.0.x, V3.1.x, V3.2.x, V4.5 and (with SSP) V4.6
- SINAMICS G120P with firmware V4.2, V4.3.0, V4.3.2, V4.4, V4.5
- SINAMICS G120P BT with firmware V4.4.1
- SINAMICS G130 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G130 with firmware V4.3.1, V4.3.2, V4.4, V4.5 and (with SSP) V4.6
- SINAMICS G150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G150 with firmware V4.3.1, V4.3.2, V4.4, V4.5 and (with SSP) V4.6
- SINAMICS GM150 with firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GM150 with firmware V4.3.1, V4.4.2, V4.5 (--> SINAMICS MV)
- SINAMICS GL150 with firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GL150 with firmware V4.3.1, V4.4.2, V4.5 (--> SINAMICS MV)
- SINAMICS S110 with firmware V4.1, V4.3.1, V4.3.2 and (with SSP) V4.4
- SINAMICS S120 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S120 with firmware V4.3.1, V4.3.2, V4.4, V4.5 and (with SSP) V4.6
- SINAMICS S150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S150 with firmware V4.3.1, V4.3.2, V4.4, V4.5 and (with SSP) V4.6
- SINAMICS SL150 with firmware V4.3.1, V4.4.2, V4.5 (--> SINAMICS MV)
- SINAMICS SM120 with firmware V4.4.2
- SINAMICS SM150i with firmware V2.4.x, V2.5.1, V2.6.2, V4.5
- SINAMICS MV with firmware (with SSP) V4.5 and (with SSP) V4.6
Further details on the supported drive systems can be found in the following Excel overview.
Installed_Devices_STARTER_DVD_43020000.xls ( 105 KB ) ( approx. 100 KB )
Optional, NEW
In order to save download time and data volume, this STARTER version V4.3 SP2 can also be downloaded and installed WITHOUT online help and WITHOUT SINAMICS S/SINAMICS integrated drives. If you do not want to use the online help, then select the "Minimized" download version.
|
Installation/download version |
Complete,
i.e. download
all SINAMICS drives
files including online help |
SINAMICS partial range,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
including online help |
SINAMICS partial range and minimized,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
WITHOUT online help |
|
Vol_1_STARTER_V43_SP2_Program.zip |
YES |
YES |
YES |
|
Vol_2a_STARTER_V43_SP2_SSPs_G110_G120.zip |
YES |
YES |
YES |
|
Vol_2b_STARTER_V43_SP2_SSPs_Family_Integrated.zip |
YES |
NO |
NO |
|
Vol_3_STARTER_V43_SP2_Helps.zip |
YES |
YES |
NO |
Procedure to install STARTER V4.3 SP2:
- Download the 2 or 3 or 4 attached ZIP files (depending on the selected download version)
- Unpack the ZIP files into a shared target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory.
- After unpacking, the shared directory must appear as follows (shown for the "complete" version):
\...\SharedDirectory\01_Readme\
\...\SharedDirectory\CD_1\
\...\SharedDirectory\CD_2\
\...\SharedDirectory\CD_3\
\...\SharedDirectory\SSP_FAMILY\
\...\SharedDirectory\SSP_G110_G120\
\...\SharedDirectory\SSP_HELP\
\...\SharedDirectory\SSP_SIMOTION_INTEGRATED\
\...\SharedDirectory\SSP_SINUMERIK_INTEGRATED\
\...\SharedDirectory\Unsupported Tools\
- Start the STARTER setup program by calling it from /CD_1/SETUP.EXE.
The readme file contains important notes on how to use the tool.
|
SINAMICS MICROMASTER STARTER V4.3 SP1 HF2 (previous Version) |
This contains version V4.3 SP1 HF2 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems. The download also contains the additive SINAMICS Support Packages in the "STARTER_V43_SP1_HF2_SSPs.zip" file:
- SSP SINAMICS V4.5
- SSP SINAMICS G120 V4.5
- SSP SINAMICS G120D V4.5
- SSP SINAMICS G120P BT V4.4.1
- SSP SINAMICS MV V4.5
- SSP SIMOTION_INT V4.5
- SSP SINUMERIK_INT V4.5
- SSP SINAMICS_SM150i V4.5
These SSPs are automatically installed by the STARTER setup when the checkboxes are activated in the selection screen form.
SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key. However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Order number: 6SL3072-0AA00-0AG0.
STARTER V4.3 SP1 HF2 supports German, English, French, Spanish and Italian.
IMPORTANT: The limitation stating that NO USS protocol is provided with 64-bit Windows 7 operating systems has been CORRECTED in this HF2 version.
The following drive systems are supported
(recently included versions compared to the previous STARTER V4.2 HF1 are marked in bold):
- MICROMASTER 4th generation
- SINAMICS DCM with firmware V1.1, V1.2 and V1.3
- SIMATIC ET200S FC with firmware V1.0.x and V3.0.x
- SIMATIC ET200pro FC with firmware V3.0.x
- SINAMICS G110 with firmware V1.0.x and V1.1.x
- SINAMICS G110D with firmware V3.3.x and V3.4.x
- SINAMICS G120 with firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x, V4.2, V4.3.0, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G120C with firmware V4.4 and (with SSP) V4.5
- SINAMICS G120D with firmware V3.0.x, V3.1.x, V3.2.x and (with SSP) V4.5
- SINAMICS G120P with firmware V4.2, V4.3.0, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G120P BT with Firmware (with SSP) V4.4.1
- SINAMICS G130 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G130 with firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G150 with firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS GM150 with firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GM150 with firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS GL150 with firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GL150 with firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS S110 with firmware V4.1, V4.3.1, V4.3.2 and (with SSP) V4.4
- SINAMICS S120 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S120 with firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS S150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S150 with firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS SL150 with firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS SM120 with firmware V4.4.2
- SINAMICS SM150i with firmware V2.4.x, V2.5.1, V2.6.2 and (with SSP) V4.5
- SINAMICS MV with firmware (with SSP) V4.5
Further details on the supported drive systems can be found in the following Excel overview.
Installed_Devices_STARTER_DVD_43010200.xls ( 100 KB )
Optional NEW
In order to save download time and data volume, STARTER version V4.3 SP1 HF2 can also be downloaded and installed WITHOUT online help. If you want to do without the online helps, select the "Minimized" download variant.
|
Installation/download variant |
Complete,
i.e. download file incl. online help |
Minimized,
i.e. download file WITHOUT online help |
|
STARTER_V43_SP1_HF2_Program.zip |
YES |
YES |
|
STARTER_V43_SP1_HF2_SSPs.zip |
YES |
YES |
|
STARTER_V43_SP1_HF2_Helps.zip |
YES |
NO |
Installation procedure:
- Download the two or three attached ZIP files (depending on the selected download variant)
- Unpack the ZIP files into a shared target directory on the hard disk. Please ensure that no spaces are contained in the entire path name of this target directory.
- After unpacking, the shared directory must appear as follows:
\...\SharedDirectory\01_Readme\
\...\SharedDirectory\CD_1\
\...\SharedDirectory\CD_2\
\...\SharedDirectory\CD_3\
\...\SharedDirectory\SSP_INT_CD1\
\...\SharedDirectory\SSP_CD1\
\...\SharedDirectory\Unsupported Tools\
- Start the STARTER setup program by calling it from /CD_1/SETUP.EXE
The Readme file contains important notes on how to use the tool.
|
SINAMICS MICROMASTER STARTER V4.3 SP1 HF5 (previous version) |
You can find HotFix 5 for STARTER version V4.3 SP1 HF2 here. Hotfix 5 involves an add-on setup to the normal STARTER setup V4.3 SP1 HF2, in which the function restrictions of STARTER version V4.3 SP1 HF2 have been resolved.
Installation of Hotfix 5 is only recommended for those customers who are affected by the following function restrictions.
- Restrictions concerning the online communication between the drive and the STARTER PC that have been resolved:
Windows 7 (64 bit) – device driver installation for the USB-USS emulation unsuccessful (AP01308651) This driver is only used for SINAMICS G120 with firmware version V4.3.2. ALL other SINAMICS G120 drives do not require this driver.
- Restrictions concerning the use of the Safety Integrated functions that have been resolved:
With the function "Save under" with the option "With reorganization (slow)" or with the option "With reorganization", the addresses F_Dest_Add are reset to their default value (AP01385374¸ AP01393807).
A PROFIsafe connection via PROFINET between the configured modules (SIMATIC S7 F-CPUs and SINAMICS S120) is not possible; combination STARTER V4.3.1.2 and Step 7 V5.5.2; (AP01405181)
- Restrictions concerning the use of the DCC SINAMICS that have been resolved:
With the function "Save under" with the option "With reorganization (slow)" or with the option "With reorganization", the drive data (DOs) and DCC charts of a project are shifted or deleted (AP01375004)
Important note regarding handling projects:
1. Open the project with STARTER V4.3.1 HF5
2. Save the project with STARTER V4.3.1 HF5
3. Then run the option "With reorganization (slow)" or the option "With reorganization".
HF5 can only be installed if STARTER V4.3 SP1 HF2 (V4.3.1.2) has already been installed on the PC. For HotFix 5, the same minimum preconditions apply as for STARTER V4.3 SP1 HF2 itself.
Procedure to install STARTER HotFix 5:
- Download the attached ZIP file
- Unzip the ZIP file to a shared target directory on your hard disk
Please ensure that there are absolutely no spaces in the complete path names of this target directory.
- After unpacking, the shared directory must appear as follows:
\...\01_Readme\
\...\CD_1\
- Start the STARTER setup program by calling it from /CD_1/SETUP.EXE.
The readme file contains important notes on how to use the tool.
Here, as individual download, you will find the SINAMICS Support Package (SSP) SINAMICS V4.6 that matches STARTER >= V4.3.1.x or SCOUT V4.3.1 HF12.
With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120, G130, S150, G150 series with firmware release V4.6 can be configured and commissioned using STARTER V4.3.1.x or SCOUT V4.3.1 HF12.
Procedure for installing SSP:
- Download the attached ZIP file
- Unzip the ZIP file to a shared target directory on your hard disk
Please ensure that there are absolutely no spaces in the complete path names of this target directory.
- After unpacking, the shared directory must appear as follows:
\...\01_Readme\
\...\CD_1\
- Start the SSP setup program by calling it from /CD_1/SETUP.EXE.
The readme file contains important notes on how to use the tool.
After installing SSP from STARTER V4.3.1.x or SCOUT V4.3.1 HF12, the following drive systems are also supported
Note on online help for function release V4.6:
To access the online help for function release V4.6, download package Vol_3_STARTER_V43_SP2_HELPS.zip and run the corresponding setup.
- After unpacking, the shared directory must appear as follows:
\...\CD_1\
\...\CD_2\
\...\SSP_HELP\...
- Start the SSP setup program by calling it from /SSP_HELP/OPT/SSP_SINAMICS_HELP_V4_6/CD_1/setup.exe.
More detailed information about STARTER V4.3.1.x itself is available under ProdIS-ID: 61585426
Here, as individual download, you will find the SINAMICS Support Package (SSP) SINAMICS G120 V4.6 that matches STARTER >= V4.3.1.x or SCOUT V4.3.1 HF12.
With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS G120 series with firmware release V4.6 can be configured and commissioned using STARTER V4.3.1.x or SCOUT V4.3.1 HF12.
Procedure for installing SSP:
- Download the attached ZIP file
- Unzip the ZIP file to a shared target directory on your hard disk
Please ensure that there are absolutely no spaces in the complete path names of this target directory.
- After unpacking, the shared directory must appear as follows:
\...\01_Readme\
\...\CD_1\
- Start the SSP setup program by calling it from /CD_1/SETUP.EXE.
The readme file contains important notes on how to use the tool.
After installing SSP from STARTER V4.3.1.x or SCOUT V4.3.1 HF12, the following drive systems are also supported
Note on online help for function release V4.6:
The online help is contained in SSP and is installed automatically.
More detailed information about STARTER V4.3.1.x itself is available under ProdIS-ID: 61585426
The SINAMICS Support Package (SSP) SINAMICS MV V4.6 suitable for STARTER >= V4.3.1.x or for SCOUT V4.3.1 HF12 can be downloaded here.
The existing SINAMICS Support Package allows you to configure and commission SINAMICS drives of the SINAMICS MV with firmware version V4.6 with STARTER V4.3.1.x or SCOUT V4.3.1 HF12.
How to install the SSPs:
- Download the attached ZIP file
- Unzip the ZIP file to a shared target directory on your hard disk
Please ensure that there are absolutely no spaces in the complete path names of this target directory.
- After unpacking, the shared directory must appear as follows:
\...\01_Readme\
\...\CD_1\
- Start the SSP setup program by calling it from /CD_1/SETUP.EXE.
The readme file contains important notes on how to use the tool.
After installing SSP from STARTER V4.3.1.x or SCOUT V4.3.1 HF12, the following drive systems are also supported
Note on online help for function release V4.6:
To access the online help for function release V4.6, download package Vol_3_STARTER_V43_SP2_HELPS.zip and run the corresponding setup.
- After unpacking, the shared directory must appear as follows:
\...\CD_1\
\...\CD_2\
\...\SSP_HELP\...
- Start the SSP setup program by calling it from /SSP_HELP/OPT/SSP_SINAMICS_HELP_V4_6/CD_1/setup.exe.
More detailed information about STARTER V4.3.1.x itself is available under ProdIS-ID: 61585426
Due to security settings, a download - as marked in the screenshot - may be classified as a security risk.
To avoid problems after the installation, zip files must be classified as harmless after downloading by clicking with right mouse button > Properties > "Unblock" button
|