show the entry list
Multi Panel -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Creating underscore with the MP270
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
WinCC flexible ES -- Creating HMI configurations -- Creating screens
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How do you create a time switch with WinCC flexible?
How do you create your own on-screen keyboard for a WinCC flexible PC Runtime Station?
How do you register an ActiveX object on the configuration computer and then incorporate it in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How can you change the tab order in WinCC flexible?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How do you configure screen selection on a Windows-based operator panel with WinCC flexible via controller job 51?
How can the display for the danger and warning area of a pointer instrument be made in color?
How do you monitor and control tags on panels on which the status/control object is not available?
Why isn't at the panel the picture number displayed properly in the picture number box after CPU startup?
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
Touch Panel / Operator Panel -- Creating HMI configurations -- Tips and tricks for configuring
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
Button as pure illuminated indicator with a TP170A
Height of a textbox in a standard configuration (ProTool V6.0)
CPU functions for S7-300 with OP7/OP17
Picture change on the TP170A as tag function
"Tahoma" is the only font that can be used with OP/TP 170A/B and C7-635
How can you implement an OP73 as a handheld?
Mobile Panels -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
"Clean Screen" function blocked with Mobile Panel 170
Evaluation of the handwheel position on the Mobile Panel 170
What should you pay attention to when configuring a project ID on the Mobile Panel 177 / 277 with battery pack?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
Part number:

Description
For various applications it might be necessary to start a system function of the HMI operator panels during running operation. This can be done either directly in the Control Panel or in Runtime using the "StartProgram" function.

Instructions
The "StartProgram" is executed by means of a button with the "Click" event. This function starts the parameterized system function.
 
No. Procedure
1

In you project you assign the "Start Program" function to a button.
 
Parameter Description
Program name Name and path of the program that is to be started.
Program parameters Parameters that are transferred to the program when started. (For example, a file that is to be used.)
Display Defines the type of display.
Wait for end of program Defines whether there is to be return to the project after the called program has ended.

The figure below shows an example of how the function parameters are to be entered in ProTool or WinCC flexible.

( 56 KB )
Fig. 01: Configuration of the function

2

For an HMI operator panel with Windows CE 3.0, you use the values from the list below as program parameters.

( 47 KB )
Fig. 02: Parameters of the Control Panel in Windows CE 3.0

Note
You can see which version of Windows CE your panel has in the "System" menu item of the Control Panel.

Remark
The call of the "Transfer" menu itemdepends on the version of Windows CE Image used. "\Windows\transferApl.cpl,0" is used in more recent versions of Image.

3

For an HMI operator panel with Windows CE 5.0, you use the values from the list below as program parameters.

( 39 KB )
Fig. 03: Parameters of the Control Panel in Windows CE 5.0

Note
You can see which version of Windows CE your panel has in the "System" menu item of the Control Panel.

Note
Since this involves accessing the system level of the device, this button should be provided with a user authorization. Notes on user administration are given in the table below.
 
FAQs on the topic of user administration Entry ID
Tips and tricks on the topic of user administration (WinCC flexible) 24456113
Getting Started for Advanced Users (Edition: 04/2006; Page 94 ff) 18656980

Additional Keywords
System settings

 Entry ID:26117046   Date:2013-01-23 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour