show the entry list
WinCC SIMATIC Logon / AUA -- Product information -- Information on SIMATIC Logon / Advanced User Administrator
Using a chip card reader, how can a default user be logged on automatically while the chip card is pulled through?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of WinCC comply with FDA regulations?
How can you configure a chip card with SIMATIC Logon, with which you can log onto each local computer?
Why isn't the group selection dialog displayed any longer in WinCC V6.2 and higher?
How can you use the "GetSignature" function as of SIMATIC Logon V1.4?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
Why isn't the user currently logged on shown at Runtime?
How can you replace the Windows on-screen keyboard of SIMATIC Logon (from V1.4) with the ProTool keyboard so as not to reach the operating system during Runtime?
How can you verify a logged on user at runtime when using SIMATIC Logon (as from V1.3)?
How can you verify a logged on user at runtime when using SIMATIC Logon up to version V1.2 SP1?
How do you call the SIMATIC Logon dialog box by means of C-Script?
The WinCC Login Box appears instead of the Logon Box in WinCC Runtime.
WinCC -- Creating HMI configurations -- Configuring Runtime
How can you lock key combinations in WinCC V7.0 SP2/WinCC (TIA Portal) with Windows 7 or Windows Server 2008?
How can you have a user-specific, user-defined screen composition displayed automatically after logging on in WinCC Runtime?
How can you increase the timeout for terminating the runtime?
How do you select the path for the picture cache yourself in WinCC and how do you use the picture cache?
How do you start a specific WinCC project depending on the user logged in when the computer is booted?
How can you have different picture to the "@Welcome.pdl" Start picture displayed at the start of Runtime?
How can you have the current picture continued to be shown when you log out of WinCC Runtime?
How can you replace the Windows on-screen keyboard of SIMATIC Logon (from V1.4) with the ProTool keyboard so as not to reach the operating system during Runtime?
How do you identify the local computer name in order to enter it in the computer list for the WinCC project?
How do you configure the WinCC Autostart when using SIMATIC NET (up to and including CD11/2003 SP1)?
How do you configure the WinCC Autostart when using SIMATIC NET (as from Edition 2005)?
How do you use the monitor keyboard of WinCC?
How can you implement login/logout via a button in a picture?
How can you execute an automatic logout after a time greater than 999 minutes?
How can you configure automatic logout in WinCC?
How can you automatically log in a default user after a reboot without using the Login Box?
With Windows Server 2000/2003, Windows 2000 Professional, Windows XP Professional and Windows Vista, what should you do if disabling the key combinations is ineffective in WinCC?
How can you replace the Windows on-screen keyboard of SIMATIC Logon (from V1.4) with the ProTool keyboard so as not to reach the operating system during Runtime?
Part number:

Instructions

Up to SIMATIC Logon V1.3 SP1 you can proceed as described in Entry ID 22613581 to call the on-screen keyboard.

From SIMATIC Logon V1.4 you have the dialog "Configure SIMATIC Logon" and in the "Logon device" tab you can choose the option "Use on-screen keyboard". 

 
Fig. 01

If the "Use on-screen keyboard" option is selected, the Windows on-screen keyboard opens automatically at Runtime when the SIMATIC Logon "Logon Dialog" opens. In this way it is also possible to log on to the system when there is no physical keyboard available (when using a Touch panel, for example).

 
Fig. 02

In many cases it is important that the operator has no access to the operating system during Runtime. This entry describes the procedure from SIMATIC Logon V1.4 onwards for replacing the default on-screen keyboard of the operating system "osk.exe" with the ProTool on-screen keyboard "TouchInputPC.exe".


Fig. 03  
No. Procedure
1 Display system files in the Windows Explorer
Make the necessary settings in the Windows Explorer to have the Windows system files displayed in the Windows Explorer.
  • In the Windows Explorer you execute the menu command "Tools > Folder Options...". The "Folder Options" dialog opens. Select the "View" tab. Make sure that the option "Hide protected operating systems files (Recommended)" is not selected.
  • Click on the "Apply to All Folders" button.
  • Click the "Apply" button and then close the dialog with the "OK" button.
2 Make a copy of "TouchInputPC.exe"
  • Open the Windows Explorer and switch to the path in which the ProTool on-screen keyboard is installed. This path can vary depending on the installation of your SIMATIC software. It might look like this:
    "C:\Program Files\SIEMENS\Common\PTTouchInput".
  • Place a copy of the "TouchInputPC.exe" file in this folder and change the name to "osk.exe".
  • Copy all the files except the "TouchInputPC.exe" file to the Windows clipboard.


    Fig. 04
3 Copy the PTTouchInput files into the Windows system directory
(In the previous step you have already copied the files to be copied to the Windows clipboard.)
  • Switch to the Windows directory "%windir%\System32\dllcache". Paste the files from the Windows clipboard into this directory.
    You can paste the files from the clipboard using the context menu command "Paste".


    Fig. 05
  • Switch to the Windows directory "%windir%\System32". Paste the files from the Windows clipboard into this directory too.

Notes

  • In path specification given above is the character string "%windir%" of the current path of your Windows installation.
    In the system there is an environment variable called "windir". This contains the complete path of the Windows installation directory.
    If you execute the Windows Start menu command "Start > Run..." and execute the command "%windir%", the Windows Explorer opens with the Windows installation directory.
  • If necessary acknowledge the "Confirm File Replace" dialog with the "Yes" or "Yes, all" button.
  • If the operating system prompts you to insert the Windows installation CD, abort this procedure and keep the unknown file versions.
  • You might have to repeat this procedure after an operating system update.

Important note for the Windows XP SP3 operating system
As from Windows XP SP3 the Windows File Protection System has been made tighter. As from this version the Siemens osk.exe file will be overwritten automatically with the Microsoft osk.exe file without you receiving any notification of this. More information is available from Microsoft at this link: http://support.microsoft.com/kb/222193.

Remedy
Change the name of the "i386" folder in the path "%windir%\ServicePackFiles". Now copy the osk.exe file provided by Siemens into the two folders specified above. Then the file will no longer be overwritten automatically with the file provided by Microsoft and you will get the "Confirm File Replace" dialog as specified above. Continue as described above. Then you can change the name of the renamed folder back to "i386".

4 Restart the computer
Restart your computer.

From SIMATIC Logon V1.5 onwards you have the dialog "Configure SIMATIC Logon" and in the "Logon device" tab you can choose the option "Use on-screen keyboard".  There you can enter the required monitor keyboard directly in the Search function (Path: C:\Program Files \Common Files\Siemens\PTTouchInput\TouchInputPC.exe).


Fig. 06

 Entry ID:25220564   Date:2012-09-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour