Various encoder types (e.g. 1XP8001-1 (HTL) and 1XP8001-2 (TTL)) can be used to sense the required speed and position signals.
The MICROMASTER 4 pulse encoder module is designed so that all of the usual digital HTL and TTL pulse encoders can be used with the MICROMASTER 430/440 series of drive inverters.
The same is true for the SINAMICS G120 with CU240S series, whereby the evaluation of the encoder signals is integrated in the CU240S.
Help when selecting cables to match 1XP8001-1 encoders is provided in the following.
Pdf encoder cable ( 636 KB )
Written by: SD CST
|