show the entry list
WinCC flexible RT -- Product information -- General information
Why does the "Lock program switching" function no longer work after upgrading from SIMATIC WinCC flexible Runtime 2008 SP2 to SP3?
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
What support does Siemens AG offer to make the use of WinCC flexible comply with FDA regulations?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
Which ports are used by WinCC flexible?
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to PCs
Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML?
Which ports are used by WinCC flexible?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How do you integrate an HMI operator panel into a local network?
What options are there in WinCC flexible for using a Multi Panel or Mobile Panel as an OPC server?
What options are there in WinCC flexible 2004 for using a multipanel as an OPC server?
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
Which ports are used by WinCC flexible?
Part number:

Configuration Notes:
The Ethernet ports are assigned by the IANA (Internet Assigned Numbers Authority). When using a firewall you must enable all the ports specified in the table. All the services listed are handled via the TCP/IP protocol, except archiving via UDP.

The following ports are used in WinCC flexible Runtime:
 
  Service Port
Web server Access to internal HTML pages (HTTP) 80
Access to internal HTML pages (HTTPS) 443 (SSL)
Sm@rtServer Connection with the Sm@rtServer

(access to the Sm@rtServer for downloading the Java applets with the Internet Explorer)
5800
Connection with the Sm@rtServer
(access to the Sm@rtServer with Internet Explorer for remote monitoring and operation)
5900
OPC

OPC via DCOM

Server Connection setup: 135
Communication dynamic 1)
Client Communication dynamic 1)
OPC via XML  (Client <=> Server) 80
Printing Printing of Windows CE panels via Ethernet 1032
Archiving Archiving on a server 2) UDP 137, 138
TCP 139
Miscellaneous Transfer via Ethernet Configuration PC dynamic 1)
Panel 2308 and 50523
Communication between S7 controller 102
Panel dynamic 1)
PROFINET IO communication 3) 34964
E-mail (SMTP server) 25
Modicon controller (Modicon channel MODBUS TCP/IP) 502

1) Dynamic port:
The Microsoft Windows operating system automatically assigns the relevant service a free port that can be between Port 1024 and 65534. You must enable this area when using a firewall.

2) Archiving:
Requirement for archiving via an Ethernet network is that the server is enabled.

3) PROFINET
Communication via PROFINET must be activated in the "Control Panel", in the "PROFINET" Settings dialog.

Note:
If you change the ports of the Sm@rtServer, you must change the links accordingly in the HTML pages used. More information on changing HTML pages is available in the Help system of WinCC flexible under "Example: Configuring an integrated web server".

 Entry ID:24534065   Date:2007-07-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour