show the entry list
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
WinCC flexible RT -- Operation and maintenance -- Diagnosing errors
When is the Runtime license not recognized with a Windows Embedded System?
What is the cause of the system error message "260045 The SIMATIC Logon user does not belong to any group or belongs to multiple groups" in WinCC flexible when the user is evidently assigned to just one group?
Message indicator continues to be displayed despite counter at zero
Why are fonts and objects shown moved on a PC Runtime system or operator panel?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Part number:

Description:
With operator panels which use the serial interface for project transfer and also for communication with the controller, no connection is set up.

The system message "No. 220008 Interface IF 1A (IF 1B) (IF 2) cannot be opened" appears in the alarm display configured or in the message window.

Remedy:
If one of these interfaces is also to be used for communication, then you must disable the "Remote Transfer" option in the Transfer Settings of the Control Panel.

Below are instructions for making the setting in the following devices:

Note:
You must select the Transfer mode explicitly for another project transfer.

The following drives are concerned:

  • Allen Bradley DF1
  • Allen Bradley DH485
  • GE Fanuc  
  • LG Glofa-GM
  • Mitsubishi FX
  • Mitsubishi Protocol 4
  • Modicon Modbus
  • Telemecanique Unitelway
  • Omron Hostlink / Multilink
  • SIMATIC 500/505 serial

Instructions for disabling the option "Remote Transfer":
 
No. OP77B
1 When you start up the operator panel select the menu "Info/Settings".
2 Navigate to the menu "Logon/Settings" and then in this menu you select the "Transfer Settings" options.
3 Select "Channel 1: serial" and click on the Enter button.
4 Disable the "Enable (remote on)" option by selecting "Enable (remote off)".

( 10 KB )
Fig. 01 - Transfer Settings OP77B

 
No. TP170A
1 When you start up the operator panel select the menu "Config".
2 In the "Transfer Settings" menu (see Fig. 02) you clear the "Remote" option check box.

( 15 KB )
Fig. 02 - Transfer Settings TP170A

 
No. OP170B, OP177B, TP170B, TP177B, Mobile Panel 170, OP270, OP277, TP270, TP277, MP270, MP270B, MP277, MP370
1 When you start up the operator panel click on the "Control Panel" button.
2 Open the "Transfer" dialog by double-clicking on the icon in the Control Panel.
3 In the "Transfer Settings" dialog window you clear the "Remote Control" option check box of "Channel 1".

( 31 KB )
Fig. 03 - Transfer Settings WinCE operator panels

 Entry ID:24516725   Date:2007-02-07