show the entry list
Hotfix 1 for SIMATIC PC DiagMonitor V3.0
Part number:

Description:
If one of the following points applies for you, then it is absolutely necessary to install the SIMATIC PC DiagMonitor V3.0 Hotfix 1.

  • Insufficient updating of the display data on the web interface.
  • In the case of an alarm incomplete display of the hard disk data on the web interface.
  • When you open the web interface a security message is displayed indicating that the Security Certificate has expired.
  • When you create your own application based on the SOLMAPI interface, an error is reported when compiling.

Remedy:
Install the Hotfix 1 for the SIMATIC PC DiagMonitor V3.0. In order to be able to install Hotfix 1 for DiagMonitor you must first install SIMATIC PC DiagMonitor V3.0. The hotfix also contains an update of the Online Help for users of the SOLMAPI developer interface. The security certificate included is only to check the functions. It is recommended to install an appropriate certificate separately for coded transfer.

Download:
 
Driver Operating system Download
HF1 DiagMonitor V3.0 Windows XP
Windows 2000
 DMHotfix_3001.zip ( 589 KB )

 Entry ID:24496636   Date:2007-01-26 
I regard this article....as helpfulas not helpful                                 
related links
Hotfix 7 for DiagMonitor V2.1 and ...
Why is no data displayed in the w ...
DiagMonitor Installation of the ...
DiagMonitor Getting Started
Hotfix 1 (Update) for SIMATIC pow ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour