show the entry list
WinCC Web Navigator -- Operation and maintenance -- Diagnosing errors
How can you disable the Protected Mode of the Internet Explorer when using the WinCC WebNavigator?
With WinCC Web Navigator, how can you have a display of which users are currently accessing the web project?
What is the meaning of the message "You must enable ActiveX Controls on your browser before you are able to install the WinCC Web Navigator Client software" and what can you do about it?
What causes the error message "Network request not supported" when starting the client Web Navigator site from the IIS?
Why do you get the error message "The maximum count of allowed users is connected to the WinCC server"?
Why aren't any tags updated on the WinCC web client?
How can you avoid the "DEMO mode" of the WinCC Web Navigator client?
Why, after migration of a WinCC project from WinCC V5.1 to WinCC V6.0 SP1, is the text originally configured no longer displayed on the Web Navigator client, but only "TEXT" in buttons and in static texts?
How can you prevent an empty page being displayed when you call the diagnostics information saved by the WinCC Web Navigator from the STATUS.HTML page?
Why, after a Microsoft update, can you no longer connect the Web Navigator clients to the Web Navigator server?
Why is there no automatic reconnect between a Web Navigator client and the Web Navigator server via a firewall or a proxy server?
Why can WinCC/Web Navigator or WinCC/Dat@Monitor clients no longer connect to the WinCC/Web Navigator or WinCC/Dat@Monitor server?
Why do you get the error message "The maximum count of allowed users is connected to the WinCC server"?
Part number:

Description
You are using WinCC V5/SP1 and Web Navigator V1.0 and you get the error message "The maximum count of allowed users is connected to the WinCC server".

Cause:

  • There is a larger number of clients connected to the WinCC server than the license permits.
    Remedy
    Upgrade the license for the Web Navigator with a power pack.
  • A license is missing: In WinCC, you are presented with a message box saying that a license is missing (all licenses are checked, not only the licenses for the Web Navigator).
    Remedy
    Procure the remaining licenses.
  • The "WebNavigatorRT.exe" file is missing in the startup list.
    Remedy
    Enter the file into the startup list of WinCC. Here, you must make sure that you specify the complete path when you enter the "WebNavigatorRT.exe"!

 Entry ID:2444186   Date:2010-02-19 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour