show the entry list
S7-200 communications modules -- Configuring and programming communication -- Setting up modem connections
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you use SINAUT MICRO SC to synchronize the real-time clock of the S7-200 CPU?
How can you ensure that all data sent from an S7-200 via GPRS is received?
How can you prevent the PROVIDER from automatically disconnecting the GPRS connection between a MD720-3 modem and SINAUT MICRO SS?
How can a GPRS connection be established to a SINAUT MICRO SC server if this has no static IP address?
How can you diagnose problems establishing a GPRS connection using SINAUT MICRO SC?
How can you safely change between GPRS mode and AT mode for SINAUT MD720-3?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
Which country ID number is to be set for countries that are not supported by the EM241 modem module?
Why can't you communicate with SCADA software (WinCC) using SIMATIC MicroComputing V1.0 and the EM241 modem module?
How can you send an SMS text using an S7-200 and EM 241?
Why doesn't outgoing communication function with the EM241 when the subprograms have been created with the modem wizard in Micro/WIN V3.2.3.17?
Why isn't any connection to the controller set up when implementing the EM241 modem module in combination with STEP 7 - Micro / WIN version V3.2.4.27 and higher?
With which SIMATIC S7-200 CPUs can you use the EM241 modem module?
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
What should you watch out for with the PPI/MPI/DP interfaces if you want to use the CP 5711 with a SIMATIC S7-200?
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
STEP 7 Micro/WIN -- Configuring and programming communication -- Using basic interfaces
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you monitor the freeport communication between an S7-200 and a serial device?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
What options exist for using the position or time data from a GPS receiver in an S7-200?
How should you set the DIP switches on the PC/PPI cable for communication with the S7-200?
Why does the menu option "USB" disappear from the list box in "Set PG/PC interface" as soon as WinCC flexible 2005 is installed if "PC/PPI Cable (PPI)" is enabled on the "Local Connection" tab?
S7-200 Cables / Memory Cards / Accessories -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
What is the function of the external memory module?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How do you implement time-controlled archiving of S7-200 data on a PC via modem connection?
How can you display S7-200 Datalog data recorded on a memory module properly in Microsoft Excel?
Error message "Fatal error or missing Hardware" when downloading STEP 7 Micro/WIN Projects with recipes onto a MMC
SINAUT - Cellular Radio Components (GSM) -- Configuring and programming communication -- Configuring connections
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you acknowledge a text message (SMS) with SINAUT ST7?
How can you send a text message (SMS) with SINAUT ST7?
How can you ensure that all data sent from an S7-200 via GPRS is received?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
Part number:

Instructions:
All the information relevant to setting up a teleservice connection between an S7-200 controller and MD 720-3 as Remote Station of a local station based on the Micro Automation Sets 21 (Entry ID: 22537809) is available in the document provided here.

Attachment 1: Teleservice_MD720-3_v1d1_en.pdf ( 1152 KB )

Note:
The SINAUT MD720-3 modem supports both GSM and GPRS communication. For GPRS communication, however, you also need the SINAUT MICRO SC software for the OPC server. For the use of teleservice only, you can also use the GSM modem SIPLUS TC65T (Entry ID: 26955813)

Keywords:
Teleservice, GSM, S7-200 CPU, Controller, MC45, Terminal, Remote connection, Communication, Service, CSD, STEP 7 Micro/WIN 

 Entry ID:24376232   Date:2008-12-08