show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Why is there no entry with the current firmware version for my module in the STEP 7 hardware catalog?
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
Industrial Ethernet network components (wireless) -- Product information -- System description
Understanding Latency between the RUGGEDCOM WIN Base Station (BS) and the RUGGEDCOM WIN Subscriber Station (MS)
How do you use the smartphone to access different functions, like web server, of automation components?
Where can you find information about the configuration and calculation of RCoax systems?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Where can you find information on the topic of PROFINET?
Industrial Ethernet network components (electrical/optical) -- Product information -- System description
How to upgrade GNU Bash on a RUGGEDCOM APE line module Linux® Version (Security Advisory SSA-860967)?
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-234763)?
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-635659)?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
How do you set the "Port Mirroring" function in the Industrial Ethernet switch SCALANCE X in order to monitor data transfer from a SCALANCE X port?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Where can you find information on the topic of PROFINET?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which devices support the "Power over Ethernet" (PoE) function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
MIB (Management Information Base) for SNMP
Dependency of bus cycle times on switch times
ET 200S (standard modules) -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which modules of the Siemens portfolio support PROFIenergy functions?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which memory cards are used in the interface modules in the ET 200 with CPU functionality?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Backing up the IM 151/CPU data on Micro Memory Card
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
ET 200M (standard modules) -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which accessories can you order for the distributed IO device ET 200M and for what do you need the accessories?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
How do you replace an IM153-2 FO?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What degree of accuracy can you obtain for plant-wide and segment-wide time stamping?
NAMUR sensors on ET200 slaves
Starting up ET200-M with analog modules
Module failure with ET200-M
What do you need the Micro Memory Card (MMC) for in the ET 200M?
Time stamping of process signal changes with IM153-2BA00
Which manuals for ET 200M are available for downloading in A&D Product Support?
ET 200eco -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which labeling signs and lettering systems are available in IP65/IP67 for the distributed IO SIMATIC ET 200?
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
ET 200pro -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which labeling signs and lettering systems are available in IP65/IP67 for the distributed IO SIMATIC ET 200?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Network transitions and links (DP) -- Product information -- System description
What do the LEDs indicate on the standard repeater?
What is the difference between "normal routing" and data record routing?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What are the requirements for operating the DP/ASi-Link Advanced as DP master on a CP 443-5 Extended?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which modules support the S7 routing function?
How do you set up the DP/PA link and how do you configure the DP/PA link and DP/PA coupler?
Unidirectional data transfer with the DP/DP coupler
Documentation for the DP/PA coupler in Dutch, Danish, Finnish, Swedish, Portuguese and Greek
S7-300 CPU 31x -- Product information -- Background and system information
How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
What is the emergency address (emergency IP) of a CPU and when is this enabled or disabled?
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when using the alarm numbering procedure?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
What is the maximum number of parameters that can be assigned to an FC and FB in the S7-300 CPU?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Why is only a warm start available for S7-300?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which entries deal with consistent data in conjunction with distributed I/O?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Status of the run-time meter after overall reset
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Local data addressing with S7-300 / S7 400
S7 300 run-time meter doesn't give any value
S7-400 CPU 41x -- Product information -- Background and system information
How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?
When compiling a CFC chart, why is the error message "Time stamp conflict" displayed in connection with the Modbus/TCP FBs for S7-400 CPUs?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Part number:

Description
The modules below have a fixed factory-set MAC address.

  • S7-300 and S7-400 Industrial Ethernet CPs
  • S7-300 and S7-400 CPUs with integrated PROFINET interface
  • Network components like SCALANCE X, SCALANCE W, SCALANCE S, PN/PN coupler
  • Gateways like IE/PB Link, IWLAN/PB Link and IE/AS-Interface Link
  • Interface modules of ET 200M, ET 200pro and ET 200S
  • ET 200eco PN

The first 3 bytes of the MAC address describe the manufacturer ID, also known as the OUI (Organizationally Unique Identifier).
Up to now these modules above have been delivered with a MAC address in which the first three bytes have always been 08-00-06.

The manufacturer ID of the MAC addresses is administered by the IEEE (Institute of Electrical and Electronics Engineers). At the link below you can see which manufacturer ID or OUI the first three bytes of a MAC address describe.

IEEE-Standards Association

SIEMENS AG uses the following manufacturer IDs or OUIs for the MAC addresses of the above-mentioned network-compatible devices.

  • 08-00-06 (hex)
    SIEMENS AG
    Siemens IT Solutions and Services, SIS GO QM O
    Siemensstraße 2-4
    POB 2353 Fürth 90713
    GERMANY
  • 00-0E-8C (hex)
    Siemens AG A&D ET
    Siemensstraße 10
    Regensburg 93055
    GERMANY
  • 00-1B-1B (hex)
    Siemens AG
    I IA SC EWK PU1, Östliche Rheinbrückenstraße 50
    76181 Karlsruhe, Baden Württemberg
    GERMANY

Confusion may arise in the following situations:

  • A network engineer uses a new module whose factory-set MAC address has the manufacturer ID 00-0E-8C or 00-1B-1B. From older modules he is used to factory-set MAC addresses having the manufacturer ID 08-00-06. Therefore he will look for a MAC address 08-00-06-xx-yy-zz which, however, he will not find.
  • Spare parts scenario: A module with a factory-set MAC address of 08-00-06-xx-yy-zz is defective and has to be replaced with a new module. It might be that the factory-set MAC address of the new module has the manufacturer ID 00-0E-8C or 00-1B-1B.

 Entry ID:24357770   Date:2011-08-22