show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
TeleService/TS/PC Adapter -- Setting up and parameterizing hardware -- Configuring devices
Which settings and parameters are required to create a gateway from GSM to ISDN with TeleService S7?
How do you parameterize the TS Adapter II / IE modems for Australia and New Zealand?
TeleService with ET200S (IM151-CPU) and TS Adapter
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
How is the TS Adapter IE parameterized for an EDI connection with the product PCAnywhere?
What should you watch out for when parameterizing the initialization string for a modem with TeleService?
How do you commission a GSM wireless modem of the type M20 Terminal with TeleService S7 V5.x?
How are remote monitoring and control performed with TeleService IE?
What are the options for using the TS Adapter IE as standard router?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you set the local modem after installing TeleService V6.1?
Check list for implementing a PC adapter
How do you commission the TS adapter V5.x with the GSM modules TC35 terminal and TC35i terminal?
Call-back feature of the TS adapter v.5.x
Connecting to the Network via Auxiliary System
S7-200 communications modules -- Configuring and programming communication -- Setting up modem connections
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you use SINAUT MICRO SC to synchronize the real-time clock of the S7-200 CPU?
How can you ensure that all data sent from an S7-200 via GPRS is received?
How can you prevent the PROVIDER from automatically disconnecting the GPRS connection between a MD720-3 modem and SINAUT MICRO SS?
How can a GPRS connection be established to a SINAUT MICRO SC server if this has no static IP address?
How can you diagnose problems establishing a GPRS connection using SINAUT MICRO SC?
How can you safely change between GPRS mode and AT mode for SINAUT MD720-3?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
Which country ID number is to be set for countries that are not supported by the EM241 modem module?
Why can't you communicate with SCADA software (WinCC) using SIMATIC MicroComputing V1.0 and the EM241 modem module?
How can you send an SMS text using an S7-200 and EM 241?
Why doesn't outgoing communication function with the EM241 when the subprograms have been created with the modem wizard in Micro/WIN V3.2.3.17?
Why isn't any connection to the controller set up when implementing the EM241 modem module in combination with STEP 7 - Micro / WIN version V3.2.4.27 and higher?
With which SIMATIC S7-200 CPUs can you use the EM241 modem module?
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
Part number:

Configuration Notes:
Taking three examples we describe the settings required to set up a connection with the TS Adapter II modem to nodes on the network, like an S7-200.

In this sample configuration we will use:

  • TS Adapter II modem (order number: 6ES7 972-0CB35-0XA0)
  • S7-200 / CPU 224
  • S7-300 / CPU 315-DP
  • TP177B
No. Example 1:
1 Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller.

( 22 KB )
Fig. 01

If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) without any other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI *) or Advanced PPI *) network type. All other settings such as Auto and PROFIBUS lead to the display of "BUSF" on the TS Adapter.

*) Notes:

  • If you configure the MPI network type on the TS Adapter II modem, "PG/PC is the only master on the network" must be enabled on the TS Adapter.
  • Advanced PPI is to be set on the TS Adapter II when there are multiple CPU2xx on the MPI/PPI network and one or multiple CPU interfaces being operated in Master mode.

 
No. Example 2:
1 Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller and a panel via MPI.

( 30 KB )
Fig. 02

If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) and  there are other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI network type.

With this setting it is possible to download a project to the panel with WinCC flexible. Furthermore, with this setting you can set up an online connection to the controller with Micro/WIN.

Note:
In some cases it might happen that the panel changes to Transfer mode when the communication interface is updated in MicroWIN
(MicroWIN > Communication > "Double-click for update").

2 Settings on the panel:
On the panel you must enable "MPI Transfer" and "Remote Control" for Transfer settings
(Start menu > Control Panel > Transfer).

 
No. Example 3:
1 Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller, an S7-300 controller and a panel via MPI.

( 37 KB )
Fig. 02

If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) and  there are other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI network type.

With this setting it is possible to download a project to the panel with WinCC flexible. Furthermore, with this setting you can set up an online connection to the controller with Micro/WIN.

Note:
In some cases it might happen that the panel changes to Transfer mode when the communication interface is updated in MicroWIN
(MicroWIN > Communication > "Double-click for update").

2 Settings on the panel:
On the panel you must enable "MPI Transfer" and "Remote Control" for Transfer settings
(Start menu > Control Panel > Transfer).

 Entry ID:24321540   Date:2007-01-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour