Configuration Notes: Taking three examples we describe the settings required to set up a connection with the TS Adapter II modem to nodes on the network, like an S7-200.
In this sample configuration we will use:
- TS Adapter II modem (order number: 6ES7 972-0CB35-0XA0)
- S7-200 / CPU 224
- S7-300 / CPU 315-DP
- TP177B
| No. |
Example 1: |
| 1 |
Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller.
 ( 22 KB )
Fig. 01
If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) without any other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI *) or Advanced PPI *) network type. All other settings such as Auto and PROFIBUS lead to the display of "BUSF" on the TS Adapter.
*) Notes:
- If you configure the MPI network type on the TS Adapter II modem, "PG/PC is the only master on the network" must be enabled on the TS Adapter.
- Advanced PPI is to be set on the TS Adapter II when there are multiple CPU2xx on the MPI/PPI network and one or multiple CPU interfaces being operated in Master mode.
|
| No. |
Example 2: |
| 1 |
Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller and a panel via MPI.
 ( 30 KB )
Fig. 02
If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) and there are other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI network type.
With this setting it is possible to download a project to the panel with WinCC flexible. Furthermore, with this setting you can set up an online connection to the controller with Micro/WIN.
Note:
In some cases it might happen that the panel changes to Transfer mode when the communication interface is updated in MicroWIN
(MicroWIN > Communication > "Double-click for update"). |
| 2 |
Settings on the panel: On the panel you must enable "MPI Transfer" and "Remote Control" for Transfer settings
(Start menu > Control Panel > Transfer). |
| No. |
Example 3: |
| 1 |
Connect TS Adapter II modem (TeleService Adapter II with integrated modem) directly with an S7-200 controller, an S7-300 controller and a panel via MPI.
 ( 37 KB )
Fig. 02
If you connect a TS Adapter II modem directly to the interface of the S7-200 (e.g. CPU224) and there are other active nodes on the network, e.g. a panel, then online communication with STEP 7 - Micro/WIN only works if the TS Adapter II modem is configured to the MPI network type.
With this setting it is possible to download a project to the panel with WinCC flexible. Furthermore, with this setting you can set up an online connection to the controller with Micro/WIN.
Note:
In some cases it might happen that the panel changes to Transfer mode when the communication interface is updated in MicroWIN
(MicroWIN > Communication > "Double-click for update"). |
| 2 |
Settings on the panel: On the panel you must enable "MPI Transfer" and "Remote Control" for Transfer settings
(Start menu > Control Panel > Transfer). |
|