show the entry list
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
Multi Panel -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Mobile Panels -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
WinCC flexible RT -- Setting up systems -- Configuring software
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you simulate the system keyboard via K or F-keys?
How do you change the date format in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you configure the WinCC Autostart for WinCC flexible Runtime?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
How do you simulate the system keyboard via K or F-keys?
Part number:

Instructions:
The system keyboard can be simulated using the SimulateSystemKey function from WinCC flexible 2005. The function is particularly useful if the operator panel does not possess a separate number block or if, for example, you use an OP177B with a touch/button combination.

By "simulating" the system keyboard, the operator, on the OP 177B for example, does not necessarily have to use the touch screen (if his hands are dirty) to set or enter values on the panel.

In this example, the "number block" was configured to the following function keys in the "Template" screen on an OP 177B (see Fig. 01).


Fig. 01

In the relevant screens you can then choose whether to use the keys, which have been configured in the "Template" screen", "locally" ("Use global assignment").


Fig. 02
 
No. Procedure
1

Click the function key to which you wish to assign the "SimulateSystemKey" function and open the key properties.

2

You can find the "SimulateSystemKey" function in the "Keyboard" system function.

3 The system key which is being simulated can be selected under the "system key" parameter.


Fig. 03

4 Runtime control:
With reference to the attached sample program, you can use the "TAB button" (K2) to switch to the individual "I/O fields".
Click "Enter" (K10) to apply the values which have been input.

All the available "functions" are listed in the file below.

Attachment 1: SystemKeys.pdf ( 10 KB )  

The attached download contains the archived WinCC flexible 2005 project with the functions described above.

Attachment 1: SimulateSystemKey.zip ( 1745 KB )

Runnability and test environment:
The example can be used on all the CPU types of SIMATIC S7-300, S7-400 and WinAC.
The following table lists the components that have been used to create this entry and verify the functions described.
 
Component Product and version designation
PC operating system Microsoft Windows XP SP2
Standard tools -
Engineering tools -
HMI software WinCC flexible 2005 SP1
HMI devices OP 177B
Controllers -
Table 1: Creation environment of the download attached

 Entry ID:24259526   Date:2006-12-13 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour