show the entry list
S7-400 CPU 41x -- Product information -- Background and system information
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
What are the requirements for using the S7 routing function and which modules can you implement?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
Part number:

Description:  
In HW Config you can enter a correction factor in the "Clock" field via CPU > Properties > Diagnostics/Clock. This affects only the CPU's hardware clock. With the correction factor you can correct a time deviation (clock is "fast" or "slow") within 24 hours. You can enter positive or negative values in ms.
The influence of the ambient temperature on the quartz frequency causes the inaccuracy. Given the large temperature range (such as in the control cabinet) within which the S7 controller can be operated, this effect is more pronounced that on wristwatches, for example.

Example:
If the clock is 4 seconds slow after 24 hours, you need to enter a correction factor of "+4000 ms".

Note:
Cycle interrupts are derived from the system clock and have nothing to do with the hardware clock settings. More information is available in the HW Config Online Help (Help button in the relevant tab of the CPU's Properties dialog).

 Entry ID:24161902   Date:2006-11-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour