Contents The procedure is given in the attached PDF document with the following contents.
- Introduction
1.1 When should you use an HMI station and when a PC station?
1.2 Which Ethernet CP should you select?
- Connecting a panel to SIMATIC S7 via Industrial Ethernet
2.1 Requirements
2.2 Configuration in STEP7 and WinCC flexible
- Connecting a WinCC flexible Runtime to SIMATIC S7 without Station Configuration Editor
3.1 Requirements
3.2 Connecting an HMI station
3.3 Connecting a PC station
- Connecting a WinCC flexible Runtime to SIMATIC S7 with Station Configuration Editor
4.1 Requirements
4.2 Connecting an HMI station
4.3 Connecting a PC station
Attachment 1: WinCC_flexible_Kommunikation_Ethernet.pdf ( 1403 KB )
|