show the entry list
STEP 7 -- Setting up development environments -- Installing and upgrading software
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Which SIMATIC software can you install in 64-bit operating systems?
Why can't STEP 7 be installed because of NCM?
Information on the topic of "Installing and upgrading software"
How do you uninstall STEP 7 completely, including all the software packages?
Tips and tricks for installing and upgrading software in STEP 7
How can you update the hardware catalog without direct internet access?
How do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards?
How can you work with two different versions of STEP 7 on one computer?
Which settings and procedures are to be observed with regard to InstallShield when installing STEP 7?
How in Windows XP/Vista/7 can you disable the message "Please reboot before installing any more programs"?
Why can the current software upgrade not be installed?
What are the requirements for installing STEP 7 version V5.5?
STEP 7 -- Product information -- System description
How does the system function SFC59 "RD-REC" behave when you read out data record 0 or 1 from an old S7-300 FM module or from an old S7-300 CP?
Where are the standard blocks and instructions stored in STEP 7 V11 (TIA Portal) and in V5.5 (SIMATIC Manager)?
What are the differences in the keyboard operation of STEP 7 Basic V10.5, V11 and STEP 7 V5.5?
What are the requirements for installing STEP 7 version V5.5?
What should you watch out for when converting from TI programs to S7 programs?
What are the essential differences between STEP 7 Lite and STEP 7 / STEP 7 Professional?
Which system functions can you use to copy data and what are the differences between the various SFCs?
What are the differences between STEP 7 and STEP 5 in the program structure?
How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5?
IEC 61131-3 and SIMATIC S7
Why can't you set up an online connection any more after installing STEP 7 version V5.4 with a PC/TS adapter?
Which details does Technical Support need regarding inquiries about SIMATIC STEP 7 software?
What are the requirements for installing STEP 7 version V5.5?
Part number:

Configuration Note:
The following table lists the requirements for installing STEP 7 version V5.5. You should observe the following points before installing the STEP 7 software:

  1. Hardware requirements
  2. Software requirements
  3. Operating systems not supported
  4. Compatibility with other software products
  5. Memory requirements
  6. User rights
  7. Installation over an existing version of STEP 7
  8. Installation of STEP 7 Professional Edition 2010

The table also includes a number of remedies if the installation is aborted or error messages are displayed during or after installation:

  1. Message: "Please reboot before installing any more programs"
  2. Message: "257:5  One or more objects of a type cannot be displayed. ..."
  3. Message: "RUNTIME ERROR 9 - Subscript out of range"
  4. Message: "Runtime Error 53"
  5. Message: "ScriptEngine too old"
  6. Message: "Internal OLE error 256:26"

Requirements and remedies for installing STEP 7 version V5.5
 
No. Requirements / Remedies
1 Hardware requirements
Please note that you need increased main memory expansion for STEP 7 version V5.5. Below are the requirements for STEP 7 V5.5.
  • In Windows XP Professional your PC requires at least 512 MB RAM and a processor of at least 600 MHz (recommended memory expansion of 1 GB).
  • In Windows Server 2003 your PC requires at least 1 GB RAM and a processor of at least 2.4 GHz.
  • In Windows 7 your PC requires at least 1 GB RAM and a processor of at least 1 GHz (recommended memory expansion of 2 GB).
2 Software requirements
STEP 7 version V5.5 is released for the operating systems below:
  • MS Windows 7 32-bit Ultimate Professional and Enterprise (standard installation) with or without SP1.
  • *MS Windows 7 64-bit Ultimate Professional and Enterprise with or without SP1.
  • *MS Windows Server 2008 R2 (64-bit) with or without SP1.
  • MS Windows XP Professional SP2 or SP3.
  • MS Windows Server 2003 SP2 / R2 SP2 standard edition as workstation computer.

The STEP 7 software is released for Windows XP Professional (32-bit). Installation in Windows XP Professional X64 (64-bit edition) is not possible.

*STEP 7 V5.5+SP1 (or higher)

Internet Explorer
You need the Internet Explorer 6.0 (or higher).

More information is also available in our FAQ on "Compatibility of STEP 7 versions with the MS Windows operating systems" in Entry ID: 8250891.

3 Operating systems not supported
Windows 95 / 98 / Me / NT / Windows 2000 and Windows Vista are no longer supported. Windows XP mode in Windows 7 is not released.
4 Compatibility with other software products
Information on this is available in our FAQ "Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.5?" in Entry ID: 18734363.
5 Memory requirements
STEP 7 V5.5 requires between about 650 and 900 MB of free memory on your hard disk.

The Windows operating systems supported require additional memory on the hard disk (typically disk C:) for the swap file, depending on the memory expansion available. You should keep at least twice the size of the main memory free. (Example: with a main memory expansion of 512 MB you need another 1024 MB of free memory on the hard disk for the swap file after installing STEP 7). Depending on the project size, you might need a larger swap file when copying an entire project, for example (twice the project size in addition on the hard disk). If the memory for the swap file is too small, errors might occur (or the program might even crash). Other Windows applications (MS Word, for example) running simultaneously with STEP 7 V5.5 also require additional hard disk space for the swap file.

More information on setting the virtual main memory in the Windows operating systems is also available in Entry ID: 20440472.

6 User rights
Unlike previous versions of STEP 7, as from STEP 7 V5.3 you only have to log on as user (no guest logon) to be able to work with STEP 7 in MS Windows 2003/XP/7. But you need administrator rights to install the STEP 7 software and install modules via the application "Set PG/PC Interface". For using options packages, please check the rights required in each case.

Notes

  • Runnability with user rights is enabled only for STEP 7 itself. Operation and user rights are not ensured for options packages. Here you might need administrator or standard user rights in addition.
  • After installing/uninstalling new hardware you must reboot the computer at least once directly with administrator rights.
7 Installation over an existing version of STEP 7
You can install STEP 7 version V5.5 over an existing installation of STEP 7 V5.1, V5.2, V5.3 or V5.4. Normally you do not need to uninstall an previous versions of STEP 7 or installed options packages beforehand. Please note, however, that STEP 7 version V5.3 no longer supports older operating systems (Windows 95/98/ME). Under circumstances it might be necessary to upgrade your operating system beforehand (see Point 2 "Software requirements"). You require a valid license for STEP 7 V3.x, V4.x, V5.0, V5.1, V5.2, V5.3 or V5.4 to install STEP 7 V5.5 Upgrade.

Make a backup of your authorizations/licenses before upgrading your operating system.

Note
You cannot install an earlier version of STEP 7 (V5.2 or V5.3, for example) over a more recent version of STEP 7 (V5.5). If you have installed version V5.5 on your computer and for a specific reason you have to downgrade again to version V5.4, for example, then you must completely uninstall STEP 7 before installing. For this refer to our FAQ "Complete uninstallation of STEP 7" in Entry ID: 189025.

8 Installation of STEP 7 Professional Edition 2010
STEP 7 Professional includes the components STEP 7, S7-GRAPH, S7-SCL and S7-PLCSIM. It has a general setup and its own authorization/license. If you already have STEP 7 software installed on your computer, you need one of the following two software packages:
  • STEP 7 Professional Upgrade
    You can install this over a STEP 7 Professional Edition 01/2000, 08/2000, 08/2001, 12/2002, 2004 or 2006 (a relevant valid authorization/license must be installed).
  • STEP 7 Professional PowerPack
    You can install this over STEP 7 V3.x, V4.x, V5.0, V5.1, V5.2, V5.3, V5.4 or V5.5 (a relevant valid authorization/license must be installed). You must have the PowerPack to be able to switch from STEP 7 to STEP 7 Professional.
9 Message: "Please reboot before installing any more programs"
If you get this error message after installing STEP 7 even though you have already rebooted your PC, we recommend referring to the following FAQ:
  • How can you clear the cause of the message "Please reboot before installing any more programs" (Windows XP/2000)?
    (Entry ID: 8861819).
10 Message: "257:5  One or more objects of a type cannot be displayed. ..."
This error message is complemented by a second error text that refers to the server or also a file that cannot be found or recognized by STEP 7. This could be due to a faulty installation or a version conflict. We recommend referring to the following FAQ:
  • "How can you clear the error message 257:5?"
    (Entry ID: 18832840).

This FAQ includes a table with the second error texts that might be displayed in this context. For each error text there is a description of the cause and how to remedy it.

11 Message: "RUNTIME ERROR 9 - Subscript out of range"
When the STEP 7 Setup is started automatically from the STEP 7 installation CD and the following message appears: "RUNTIME ERROR 9 - Subscript out of range", then most likely the file "INSTDUMP.TMP" on C:\ on your computer has an old date. This file was created by an earlier Setup. It is created when the Setup is not terminated correctly (PC/PG crash or error during installation, for example).

Remedy
Delete the "INSTDUMP.TMP" file located directly on the "C:\" drive.

12 Message: "Run Time Error 53"
In some cases the CD-ROM or DVD drives have problems reading and extracting installation files from the STEP 7 CD. This message appears at the start of the Setup from the CD in an external CD-ROM drive. If you have the possibility of procuring a new CD-ROM driver from the manufacturer, then you should replace your 16-bit-mode driver with a more recent 32-bit-mode driver. This will then clear this behavior. Otherwise proceed as follows.
  • Copy the CD contents to a local or network drive and start Setup from there.
  • If this is likewise not possible, you can also start the Setup for STEP 7 or NCM directly from the directory concerned.

More reasons
If the Setup is executed on an operating system on which no default language is installed (DE, EN, FR, for example), the "Runtime error: 53" message: might also appear, because various files cannot be read because of the language-dependent ASCII character table.

Remedy

  • Copy the CD contents to a local or network drive and delete all the files that contain such ASCII characters. Since these characters are usually mainly in attached *.PDF files, you should now be able to install the software.
  • To install the software set your operating system to a default language (DE, EN, FR).
13 Message: "ScriptEngine too old"
If installation of the STEP 7 software is aborted with the message "ScriptEngine too old", we recommend referring to the following two FAQs for a remedy:
  • How do you install STEP 7 when the installation is aborted with an InstallShied error? (Entry ID: 17420236),
  • "Default properties of the DCOM interface under MS Windows XP" (Entry ID: 16503255).

If none of the remedies in these two FAQs is successful, we recommend proceeding as follows:

  • Empty all the temporary directories on your system.
  • In Windows under "Start > Run..." enter "msiexec /unreg" and click on OK.
  • Repeat this step and enter "msiexec /regserver".
  • Delete the directory ...\Installshield\driver\8 (if it exists).
  • Open the file ISScript8.Msi and follow the on-screen instructions. This file is located on the STEP 7 CD in the "IS" directory.

Then you can install STEP 7 via the Setup program (Setup.exe).

14 Message: "Internal OLE error 256:26"
If this message is displayed during or after installing the STEP 7 software or even when opening the SIMATIC Manager or any STEP 7 blocks, then we recommend referring to the following FAQ:
  • Notes on error message 256:26 "An OLE error has occurred" (Entry ID: 10208766)

More information is available in the readme file of STEP 7 V5.5. This file is located

  • On the STEP 7 CD in the "STEP7\Disk1" directory (file: README.WRI).
  • After installing STEP 7, in Windows under "Start > SIMATIC > Information > English > STEP 7 - Readme".

Keywords
System requirements, System performance, Setup

 Entry ID:24059046   Date:2012-02-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour