show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
ProTool -- Configuring and programming communication -- Configuring communication to S7
Settings in "Status/Force" when using a WinAC MP
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
Connecting a panel to a S7 300/400 controller
Connection settings for a communication between ProTool/Pro and WinAC
How can you increase the performance of HMI devices?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
ProTool/ProRT and S7-200 with PC/PPI-Cable
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Coupling between ProTool/Pro and WinAC
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
Part number:

 
Description:
The FAQ concerns those FMs that exchange data with an HMI device. The following modules are concerned:
 
FM type MLFB
FM353  F. STEPPER MOTOR 6ES7353-1AH01-0AE0
FM354  F. SERVO MOTOR 6ES7354-1AH01-0AE0
FM357  4 AXIS CONTROL 6ES7357-4AH01-0AE0

CPU-dependent FM addressing
In the S7-300 CPUs there are two different architecture models with regard to the bus, in which the FM addressing is displayed differently to the user in each case. A difference is to be made between CPUs with and without combined MPI/DP interface.

  • CPUs without combined MPI/DP interface
    In HW Config the MPI address "MPI addr.[CPU] + 1" is entered automatically for the FM module. This value could also be changed by the user if necessary.


    Fig. 01


    This case holds for all configurations with CPUs that are not included in the table below.
     
  • CPUs with combined MPI/DP interface
    In HW Config the MPI address of the FM module is not displayed. The user does not know which FM address is to be parameterized in the HMI configuration tool.


    Fig. 02


    This case holds for all configurations with CPUs that are included in the table below.
     
CPUs with integrated DP interface

CPU 315-2 PN/DP

CPU 315F-2 PN/DP
CPU 317 (all types)
CPU 318 (all types)
CPU 319 (all types)

HMI <-> FM connection configuration for CPUs without combined MPI/DP interface:
(address data of the following examples (screenshots): CPU: MPI=2, Slot=2; FM: MPI=3, Slot=4;)

Connection configuration with ProTool or WinCC flexible permits two access paths to the FM:

  • Access path 1


    Fig. 03



    Fig. 04

  • Access path 2


    Fig. 05



    Fig. 06
     

HMI <-> FM connection configuration for CPUs with combined MPI/DP interface:
(address data of the following examples (screenshots): CPU: MPI=2, Slot=2; FM: Slot=4;)

  • There is only Access path 1 to the FM.


    Fig. 07



    Fig. 08
     

Note:
For the examples in the masks above the configuration tool concerned was integrated in each case in STEP 7. In these cases entry of the FM address (MPI, slot and BGT numbers) is automatic and cannot be changed by the user as long as you click to select the FM or access point via which the FM is to be reached. Manual input of the FM address data is possible by clicking "Define the parameters yourself" (ProTool) or "No station" for station selection (WinCC flexible). In the case of a nonintegrated configuration tool you must always specify the FM address data manually.

 Entry ID:23977876   Date:2006-10-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour